Does CubeMX -F4x freeRTOS/LWIP actually work?
I created a project for the Nucleo-F207 board using FreeRTOS and LWIP that worked. But when I tried to re-create the same project for the -F429 it did NOT work. [However the -F207 binary did work when loaded on the -F429 board.] On the -F429, DHCP only half worked; it sent out a Discovery message but did not accept the OFFER message. I have not pursued what the problem is yet.
I noticed that cubeMX used different versions of both FreeRTOS and LWIP for the two different processors.
My question:
Can anyone confirm that the code produced by cubeMX for -F4xx/FreeRTOS/ LWIP actually works?
... or should I just build my -F429 project off the -F207 code base?