Does STM32Cube_FW_H5_V1.2.0 MCU package suppolrt FREERTOS?
Greetings,
I am using a NUCLEO-H563ZI with the STM32CubeIDE, and wanted to create a new project based on
FREERTOS. It appears that FREERTOS is not part of this release, and the tools tell me I have to download it.
1) Is there a version on FREERTOS compatible with STM32Cube_FW_H5_V1.2.0?
2) I see that STM32Cube_FW_H5_V1.2.0 supports ThreadX, is ST moving away from FREERTOS support in
favor of ThreadX?
3) How can I download and install FREERTOS into STM32Cube_FW_H5_V1.2.0?
Thanks
Ken