Does USB library work under heavy interrupt load?
I'm implementing a USB Host (HID Class) on a STM32F7 in order to connect a mouse.
The problem is that in about 50% of cases, phost->gState ends up in HOST_ABORT_STATE, where exactly I do not know. If this does not happen, my user function USBH_HID_EventCallback() is never called more than once.
What is special about my setting is that I have external interrupts enabled, which trigger about every half microsecond when under load. The STM32 keeps up with that, but I wonder if those interrupts might interfere with the USB library, especially the low-level parts dealing with signals.
Does anybody have any insights on how the USB library deals with interrupts? Will it disable interrupts for critical sections? Is there a recommendation how often USBH_Process() should be called?