DS2431 Read ROM returns 0x00 on STM32F446RE
Post edited by ST moderator to be inline with the community rules especially with the code sharing. In next time please use </> button to paste your code. Please read this post: How to insert source code
Hi everyone,
I’m trying to communicate with a Maxim DS2431 (1-Wire EEPROM) using an STM32F446RE MCU.
I can successfully generate the reset and sometimes detect a presence pulse, but when I send the Read ROM (0x33) command, the data I receive is always 0x00 for all 8 bytes.
I’m implementing the 1-Wire protocol manually (bit-banging) using a GPIO pin.
Below are the hardware details and what I’ve tried so far.
🧱 Hardware setup
-
MCU: STM32F446RE @ 180 MHz
-
DS2431 powered at 3.3V (not parasitic)
-
1-Wire line connected to: GPIOA_PIN_0
-
Pull-up resistor: tried 2.2kΩ and 1.8
Is there anyone who has worked with DS2431 on STM32 before and can share experience, timing details, or working example code?
Thanks in advance :folded_hands:
Here is my 1-Wire read implementation:```c
/* USER CODE BEGIN Header */ /* USER CODE END Header */ /* Includes ------------------------------------------------------------------*/ #include "main.h" /* Private includes ----------------------------------------------------------*/ /* USER CODE BEGIN Includes */ #define DS2431_PORT GPIOA #define DS2431_PIN GPIO_PIN_0 #include "string.h" #include "stdio.h" /* USER CODE END Includes */ /* Private typedef -----------------------------------------------------------*/ /* USER CODE BEGIN PTD */ /* USER CODE END PTD */ /* Private define ------------------------------------------------------------*/ /* USER CODE BEGIN PD */ /* USER CODE END PD */ /* Private macro -------------------------------------------------------------*/ /* USER CODE BEGIN PM */ extern UART_HandleTypeDef huart2; /* USER CODE END PM */ /* Private variables ---------------------------------------------------------*/ TIM_HandleTypeDef htim1; UART_HandleTypeDef huart2; /* USER CODE BEGIN PV */ /* USER CODE END PV */ /* Private function prototypes -----------------------------------------------*/ void SystemClock_Config(void); static void MX_GPIO_Init(void); static void MX_USART2_UART_Init(void); static void MX_TIM1_Init(void); /* USER CODE BEGIN PFP */ /* USER CODE END PFP */ /* Private user code ---------------------------------------------------------*/ /* USER CODE BEGIN 0 */ void usDelay(uint16_t us) { __HAL_TIM_SET_COUNTER(&htim1, 0); // Counter'ı sıfırla while (__HAL_TIM_GET_COUNTER(&htim1) < us); // Bekle } void OneWire_OutputLow(void) { GPIO_InitTypeDef GPIO_InitStruct = {0}; GPIO_InitStruct.Pin = DS2431_PIN; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_OD; GPIO_InitStruct.Pull = GPIO_NOPULL; HAL_GPIO_Init(DS2431_PORT, &GPIO_InitStruct); HAL_GPIO_WritePin(DS2431_PORT, DS2431_PIN, GPIO_PIN_RESET); } void OneWire_Release(void) { GPIO_InitTypeDef GPIO_InitStruct = {0}; GPIO_InitStruct.Pin = DS2431_PIN; GPIO_InitStruct.Mode = GPIO_MODE_INPUT; GPIO_InitStruct.Pull = GPIO_NOPULL; HAL_GPIO_Init(DS2431_PORT, &GPIO_InitStruct); } uint8_t OneWire_ReadPin(void) { return HAL_GPIO_ReadPin(DS2431_PORT, DS2431_PIN); } /* ------------------------------------------------------------- * 1-WIRE RESET + PRESENCE DETECT * ------------------------------------------------------------- */ uint8_t OneWire_Reset(void) { uint8_t presence = 1; // varsayılan: cihaz yok // Hat LOW yap OneWire_OutputLow(); usDelay(480); // Reset pulse // Hat HIGH (release) OneWire_Release(); usDelay(70); // Wait before presence check // Presence okuyalım (0 = device present) if (OneWire_ReadPin() == GPIO_PIN_RESET) presence = 0; usDelay(410); // Wait for end of timeslot return presence; // 0 = presence detected, 1 = no device } /* ------------------------------------------------------------- * 1-WIRE WRITE BIT * ------------------------------------------------------------- */ /* ------------------------------------------------------------- * 1-WIRE READ BIT * ------------------------------------------------------------- */ uint8_t OneWire_ReadBit(void) { uint8_t bit = 0; OneWire_OutputLow(); usDelay(6); OneWire_Release(); usDelay(9); bit = OneWire_ReadPin(); usDelay(55); return bit; } uint8_t OneWire_ReadByte(void) { uint8_t data = 0; for (int i = 0; i < 8; i++) { // Doğru bit pozisyonuna yerleştir data >>= 1; if (OneWire_ReadBit()) data |= 0x80; // usDelay(1); // Bu satırı KALDIR - zaten ReadBit içinde delay var } return data; } void OneWire_WriteBit(uint8_t bit) { if (bit) { OneWire_OutputLow(); usDelay(6); OneWire_Release(); usDelay(64); } else { OneWire_OutputLow(); usDelay(60); OneWire_Release(); usDelay(10); } } void OneWire_WriteByte(uint8_t data) { for (int i = 0; i < 8; i++) { OneWire_WriteBit(data & 0x01); data >>= 1; } } void OneWire_ReadROM(uint8_t *romData) { if (OneWire_Reset() == 0) // Presence kontrolü { OneWire_WriteByte(0x33); // Read ROM komutu for (int i = 0; i < 8; i++) { romData[i] = OneWire_ReadByte(); } } else { } } /* USER CODE END 0 */ /** * @brief The application entry point. * @retval int */ int main(void) { /* USER CODE BEGIN 1 */ /* USER CODE END 1 */ /* MCU Configuration--------------------------------------------------------*/ /* Reset of all peripherals, Initializes the Flash interface and the Systick. */ HAL_Init(); /* USER CODE BEGIN Init */ /* USER CODE END Init */ /* Configure the system clock */ SystemClock_Config(); /* USER CODE BEGIN SysInit */ /* USER CODE END SysInit */ /* Initialize all configured peripherals */ MX_GPIO_Init(); MX_USART2_UART_Init(); MX_TIM1_Init(); /* USER CODE BEGIN 2 */ uint8_t rom[8]; char buffer[100]; /* USER CODE END 2 */ /* Infinite loop */ /* USER CODE BEGIN WHILE */ while(1){ // HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_5); // usDelay(1000); if (OneWire_Reset() == 0) { // Presence detected HAL_GPIO_WritePin(GPIOA, GPIO_PIN_5, GPIO_PIN_SET); OneWire_ReadROM(rom); sprintf(buffer, "ROM = "); HAL_UART_Transmit(&huart2, (uint8_t*)buffer, strlen(buffer), HAL_MAX_DELAY); for (int i = 0; i < 8; i++) { sprintf(buffer, "%02X ", rom[i]); HAL_UART_Transmit(&huart2, (uint8_t*)buffer, strlen(buffer), HAL_MAX_DELAY); } sprintf(buffer, "\r\n"); HAL_UART_Transmit(&huart2, (uint8_t*)buffer, strlen(buffer), HAL_MAX_DELAY); } else { HAL_GPIO_WritePin(GPIOA, GPIO_PIN_5, GPIO_PIN_RESET); // No device } } // if (OneWire_Reset()) // { // OneWire_ReadROM(rom); // // sprintf(buffer, "ROM = "); // HAL_UART_Transmit(&huart2, (uint8_t*)buffer, strlen(buffer), HAL_MAX_DELAY); // // for (int i = 0; i < 8; i++) // { // sprintf(buffer, "%02X ", rom[i]); // HAL_UART_Transmit(&huart2, (uint8_t*)buffer, strlen(buffer), HAL_MAX_DELAY); // } // // sprintf(buffer, "\r\n"); // HAL_UART_Transmit(&huart2, (uint8_t*)buffer, strlen(buffer), HAL_MAX_DELAY); // } // else // { // char msg[] = "No presence detected.\r\n"; // HAL_UART_Transmit(&huart2, (uint8_t*)msg, strlen(msg), HAL_MAX_DELAY); // } // // HAL_Delay(1000); // } /* USER CODE END WHILE */ /* USER CODE BEGIN 3 */ /* USER CODE END 3 */ } /** * @brief System Clock Configuration * @retval None */ void SystemClock_Config(void) { RCC_OscInitTypeDef RCC_OscInitStruct = {0}; RCC_ClkInitTypeDef RCC_ClkInitStruct = {0}; /** Configure the main internal regulator output voltage */ __HAL_RCC_PWR_CLK_ENABLE(); __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1); /** Initializes the RCC Oscillators according to the specified parameters * in the RCC_OscInitTypeDef structure. */ RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI; RCC_OscInitStruct.HSIState = RCC_HSI_ON; RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON; RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI; RCC_OscInitStruct.PLL.PLLM = 8; RCC_OscInitStruct.PLL.PLLN = 180; RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2; RCC_OscInitStruct.PLL.PLLQ = 2; RCC_OscInitStruct.PLL.PLLR = 2; if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) { Error_Handler(); } /** Activate the Over-Drive mode */ if (HAL_PWREx_EnableOverDrive() != HAL_OK) { Error_Handler(); } /** Initializes the CPU, AHB and APB buses clocks */ RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2; RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK; RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4; RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2; if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5) != HAL_OK) { Error_Handler(); } } /** * @brief TIM1 Initialization Function * @PAram None * @retval None */ static void MX_TIM1_Init(void) { /* USER CODE BEGIN TIM1_Init 0 */ /* USER CODE END TIM1_Init 0 */ TIM_ClockConfigTypeDef sClockSourceConfig = {0}; TIM_MasterConfigTypeDef sMasterConfig = {0}; /* USER CODE BEGIN TIM1_Init 1 */ /* USER CODE END TIM1_Init 1 */ htim1.Instance = TIM1; htim1.Init.Prescaler = 100-1; htim1.Init.CounterMode = TIM_COUNTERMODE_UP; htim1.Init.Period = 0xffff-1; htim1.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1; htim1.Init.RepetitionCounter = 0; htim1.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_ENABLE; if (HAL_TIM_Base_Init(&htim1) != HAL_OK) { Error_Handler(); } sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL; if (HAL_TIM_ConfigClockSource(&htim1, &sClockSourceConfig) != HAL_OK) { Error_Handler(); } sMasterConfig.MasterOutputTrigger = TIM_TRGO_UPDATE; sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE; if (HAL_TIMEx_MasterConfigSynchronization(&htim1, &sMasterConfig) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN TIM1_Init 2 */ HAL_TIM_Base_Start(&htim1); /* USER CODE END TIM1_Init 2 */ } /** * @brief USART2 Initialization Function * @PAram None * @retval None */ static void MX_USART2_UART_Init(void) { /* USER CODE BEGIN USART2_Init 0 */ /* USER CODE END USART2_Init 0 */ /* USER CODE BEGIN USART2_Init 1 */ /* USER CODE END USART2_Init 1 */ huart2.Instance = USART2; huart2.Init.BaudRate = 9600; huart2.Init.WordLength = UART_WORDLENGTH_8B; huart2.Init.StopBits = UART_STOPBITS_1; huart2.Init.Parity = UART_PARITY_NONE; huart2.Init.Mode = UART_MODE_TX_RX; huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE; huart2.Init.OverSampling = UART_OVERSAMPLING_16; if (HAL_UART_Init(&huart2) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN USART2_Init 2 */ /* USER CODE END USART2_Init 2 */ } /** * @brief GPIO Initialization Function * @PAram None * @retval None */ static void MX_GPIO_Init(void) { GPIO_InitTypeDef GPIO_InitStruct = {0}; /* USER CODE BEGIN MX_GPIO_Init_1 */ /* USER CODE END MX_GPIO_Init_1 */ /* GPIO Ports Clock Enable */ __HAL_RCC_GPIOC_CLK_ENABLE(); __HAL_RCC_GPIOH_CLK_ENABLE(); __HAL_RCC_GPIOA_CLK_ENABLE(); /*Configure GPIO pin Output Level */ HAL_GPIO_WritePin(GPIOA, GPIO_PIN_0, GPIO_PIN_SET); /*Configure GPIO pin Output Level */ HAL_GPIO_WritePin(GPIOA, GPIO_PIN_5, GPIO_PIN_RESET); /*Configure GPIO pin : PA0 */ GPIO_InitStruct.Pin = GPIO_PIN_0; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_OD; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); /*Configure GPIO pin : PA5 */ GPIO_InitStruct.Pin = GPIO_PIN_5; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); /* USER CODE BEGIN MX_GPIO_Init_2 */ /* USER CODE END MX_GPIO_Init_2 */ } /* USER CODE BEGIN 4 */ /* USER CODE END 4 */ /** * @brief This function is executed in case of error occurrence. * @retval None */ void Error_Handler(void) { /* USER CODE BEGIN Error_Handler_Debug */ /* USER CODE END Error_Handler_Debug */ } #ifdef USE_FULL_ASSERT /** * @brief Reports the name of the source file and the source line number * where the assert_param error has occurred. * @PAram file: pointer to the source file name * @PAram line: assert_param error line source number * @retval None */ void assert_failed(uint8_t *file, uint32_t line) { /* USER CODE BEGIN 6 */ /* USER CODE END 6 */ } #endif /* USE_FULL_ASSERT */```