Eeprom Emulation on STM32H723
Hello, i am trying to implement Eeprom Emulation on STM32H723 using the code that ST provided in STM32CubeH7-Master for STM32H743 series. In the EE_Init function, first thing that function does is this line of code:
PageStatus0 = (*(__IO uint16_t*)PAGE0_BASE_ADDRESS); #define PAGE0_BASE_ADDRESS ((uint32_t)(EEPROM_START_ADDRESS + 0x0000))
when i look at the value of PAGE0_BASE_ADDRESS, it corresponds to 6U+0x000. Is that normal? Doesnt this mean that we are reading from ITCM RAM?