Enc424J600 with STM32L431 interface
Hello Team,
I need your support to integrate the Enc424J600 ethernet IC with STM32L431, I have enabled the SPI line and trying to communicate with IC but I am not able to read the register value from the Enc424J600 chip.
Ethernet State:
Status led is blinking.
SPI init:
static void MX_SPI2_Init(void)
{
/* USER CODE BEGIN SPI2_Init 0 */
/* USER CODE END SPI2_Init 0 */
/* USER CODE BEGIN SPI2_Init 1 */
/* USER CODE END SPI2_Init 1 */
/* SPI2 parameter configuration*/
hspi2.Instance = SPI2;
hspi2.Init.Mode = SPI_MODE_MASTER;
hspi2.Init.Direction = SPI_DIRECTION_2LINES;
hspi2.Init.DataSize = SPI_DATASIZE_8BIT;
hspi2.Init.CLKPolarity = SPI_POLARITY_LOW;
hspi2.Init.CLKPhase = SPI_PHASE_1EDGE;
hspi2.Init.NSS = SPI_NSS_SOFT;
hspi2.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_16;
hspi2.Init.FirstBit = SPI_FIRSTBIT_MSB;
hspi2.Init.TIMode = SPI_TIMODE_DISABLE;
hspi2.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
hspi2.Init.CRCPolynomial = 7;
hspi2.Init.CRCLength = SPI_CRC_LENGTH_DATASIZE;
hspi2.Init.NSSPMode = SPI_NSS_PULSE_ENABLE;
if (HAL_SPI_Init(&hspi2) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN SPI2_Init 2 */
/* USER CODE END SPI2_Init 2 */
}
Enc function:
static uint8_t currentBank = 0;
uint8_t TxData[8],RxData[10];
void enc624j600_setBank(uint8_t bank)
{
if (bank != currentBank)
{
HAL_GPIO_WritePin(ETH_SPI_SEL_GPIO_Port, GPIO_PIN_14, GPIO_PIN_RESET);
TxData[0] = (0b11000000 | (bank<<1));
HAL_SPI_Transmit(&hspi2,&TxData[0],1,200);
HAL_GPIO_WritePin(ETH_SPI_SEL_GPIO_Port, GPIO_PIN_14, GPIO_PIN_SET);
currentBank = bank;
}
}
void enc624j600SpiWriteRegister8(uint8_t addr, uint8_t value)
{
if ((addr & regGlobal) == 0)
{
enc624j600_setBank(addr >> 5);
}
TxData[0] = (1<<6) | (addr & 0b11111);
TxData[0] = value;
HAL_GPIO_WritePin(ETH_SPI_SEL_GPIO_Port, GPIO_PIN_14, GPIO_PIN_RESET);
HAL_SPI_Transmit(&hspi2,&TxData[0],2,200);
HAL_GPIO_WritePin(ETH_SPI_SEL_GPIO_Port, GPIO_PIN_14, GPIO_PIN_SET);
}
void enc624j600SpiWriteRegister16(uint8_t addr, uint16_t value)
{
enc624j600SpiWriteRegister8(addr, value & 0xFF);
enc624j600SpiWriteRegister8(addr+1, value >> 8);
}
uint8_t enc624j600SpiReadRegister8(uint8_t addr)
{
uint8_t dat = 0;
if ((addr & regGlobal) == 0)
{
enc624j600_setBank(addr >> 5);
}
TxData[0] = (addr & 0b11111);
TxData[0] = 0;
HAL_GPIO_WritePin(ETH_SPI_SEL_GPIO_Port, GPIO_PIN_14, GPIO_PIN_RESET);
HAL_SPI_Transmit(&hspi2,&TxData[0],1,200);
HAL_SPI_Receive(&hspi2,&RxData[0],1,200);
//HAL_SPI_TransmitReceive(&hspi2,&TxData[0],RxData,1,200);
HAL_GPIO_WritePin(ETH_SPI_SEL_GPIO_Port, GPIO_PIN_14, GPIO_PIN_SET);
return dat;
}
uint16_t enc624j600SpiReadRegister16(uint8_t addr)
{
uint16_t dat = enc624j600SpiReadRegister8(addr)
| (enc624j600SpiReadRegister8(addr+1) << 8);
printf("%04x\n",dat);
return dat;
}
void encinit(uint8_t* macaddr)
{
enc624j600WriteRegister16(EUDAST, 0x1234);
enc624j600ReadRegister16(EUDAST)!=0x1234)
{
enc624j600WriteRegister16(EUDAST, 0x1234);
osDelay(1000);
}
}
Main code:
void StartDefaultTask(void *argument)
{
/* USER CODE BEGIN 5 */
uint8_t mac[] = {0x23,0x23,0xae,0x24,0x24,0x25};
encinit(mac);
/* Infinite loop */
for(;;)
{
osDelay(1000);
}
/* USER CODE END 5 */
}
Enc header data:
Attachment
Output: Trying to read the reset data from enc, receive data: 0000h
Reference :