Question
Error in documentation in stm32u5xx_hal.adc.h
There is a little error on documention at the following lines
#define ADC_LOW_POWER_NONE (0x00000000UL) /*!< Both Low Power Auto Off and Deep Power Down is Disabled*/
#define ADC_LOW_POWER_AUTOFF (ADC4_PW_AUTOFF) /*!< Low Power Auto Off Enabled and Deep Power Down is Disabled*/
#define ADC_LOW_POWER_DPD (ADC4_PW_DPD) /*!< Low Power Auto Off Disabled and Deep Power Down is Enabaled*/
#define ADC_LOW_POWER_AUTOFF_DPD (ADC4_PW_AUTOFF | ADC4_PW_DPD) /*!< Low Power Auto Off Disabled and Deep Power Down is Enabaled*/Line 3 has to be corrected, from "Enabaled" to "Enabled"
Line 4 has to be corrected with the following sentence : "Both Low Power Auto Off and Deep Power Down are Enabled"