Error: "stm32h7xx_hal_eth.h" no such file or directory
Hello,
I am facing a problem that I am unable to solve.
My environment: 2 PCs with Cube v1.13.1 installed and working but one is not connected to internet (have to). I am working with the SMT32H750B-DK eval board and the STM32 MCU package for H7 Series v1.11.0. I am only programming on the offline PC.
My work: I am working on configuring Ethernet protocol on this board to allow me to transfer data using LwIP stack according to this tuto https://community.st.com/t5/stm32-mcus/how-to-create-project-for-stm32h7-with-ethernet-and-lwip-stack/ta-p/49308
After configuring the pins, clock and LwIP stack, Cube tries to generate the related code and asks me to provide it the H7 Series v1.11.1 package. I dl and install it on the online PC and paste it in the Repository folder of the other PC.
On the offline PC, the build set this error: fatal error: "stm32h7xx_hal_eth.h" no such file or directory
Anyway, the compiler does not recognize the new dependency added previously. Do someone has an idea how to solve this problem ?
I also tried to install the zipped dependency using the "From Local" option of the Package Manager; that failed.
Best regards.