Skip to main content
Explorer II
November 19, 2024
Solved

ETH LwIP program runs only when debugging

  • November 19, 2024
  • 2 replies
  • 1594 views

Hello ST Community!

I have a problem and I need your help. I have searched and read most of the related articles but couldn't find a solution! I am using:

  • Hardware: Nucleo H755 board connected directly to the computer.
  • Software: STM32CubeMX version 6.12 and MDK-ARM compiler version 5.41

I have carefully read the article: https://community.st.com/t5/stm32-mcus/how-to-create-a-project-for-stm32h7-with-ethernet-and-lwip-stack/ta-p/49308 and some other related tutorials, as well as related comments. I have followed the following steps.

  1. Configure according to the instructions for CM7 core, no RTOS used.
  2. Generate code (MDK Toolchain; min version 5.32).
  3. Add MX_LWIP_Process to the main loop.
  4. Compiling with the option [ARM Compiler: Use default compiler version 5] results in an unusually very slow compilation time.
  5. Compile with option [ARM Compiler: Use default compiler version 6] then compile time is normal but there is an error: ../Middlewares/Third_Party/LwIP/system\arch/cc.h(50): error: 'sys/time.h' file not found

I have fixed this error according to: https://github.com/STMicroelectronics/STM32CubeF4/issues/29 specifically:

  • In file cc.h, line 43:

#if defined (GNUC) & !defined (__CC_ARM)

is corrected to

#if defined (GNUC) && !defined (__CC_ARM) && !(defined(__ARMCC_VERSION) && (__ARMCC_VERSION >= 6010050))

  • In file lwip.c, line 25 and 178,

#if defined ( __CC_ARM )

is corrected to

#if defined (__ARMCC_VERSION) && (__ARMCC_VERSION >= 6100100)

And then, I compile and there is a warning in the ethernetif.c file, line 124: __attribute__((section(".Rx_PoolSection"))) extern u8_t memp_memory_RX_POOL_base[];

I corrected it to

__attribute__((section(".Rx_PoolSection"))) u8_t memp_memory_RX_POOL_base[];

extern u8_t memp_memory_RX_POOL_base[];

 

6. In the Scatter file I added the content for RW_DMARxDscrTab, RW_DMATxDscrTab and memory_RX_POOL_base

7. Compile successfully without error and warning

8. Download program to MCU, check ping from PC and get the result: Destination host unreachable.

9. Enter debug mode, press Run (F5) 3 time, the program runs and pings from PC successfully: bytes=32 time=1ms TTL=255.

I set the breakpoint at the beginning of the main function, I have to press the Run button 3 times before the cursor stops at this breakpoint.

10. If I press the hard reset button or turn off the power, the program does not run.

Please show me my mistakes and how to fix them! I'm a newbie. Thank you very much!

 

 

    This topic has been closed for replies.
    Best answer by Guillaume K

    Typically this happens when the application tries to use C library functions (like printf()) that use semi-hosting.

    Semi hosting requires the debugger to do some actions like getting the string from the MCU (through debugger link) and printing it in the IDE .

    When running without the debugger, the project must be compiled without semi hosting.

    one possible way on MDK-ARM to disable semi hosting is to select "Use micro-lib" in "code generation" in Target tab of your project config.

    The C library "micro-lib" doesn't use semi hosting. The printf() won't work.

    Another way would be to replace the standard library functions with one that doesn't use semi hosting.

     

    2 replies

    ST Employee
    November 19, 2024

    Typically this happens when the application tries to use C library functions (like printf()) that use semi-hosting.

    Semi hosting requires the debugger to do some actions like getting the string from the MCU (through debugger link) and printing it in the IDE .

    When running without the debugger, the project must be compiled without semi hosting.

    one possible way on MDK-ARM to disable semi hosting is to select "Use micro-lib" in "code generation" in Target tab of your project config.

    The C library "micro-lib" doesn't use semi hosting. The printf() won't work.

    Another way would be to replace the standard library functions with one that doesn't use semi hosting.

     

    TonyRuanAuthor
    Explorer II
    November 19, 2024

    Thanks for your reply, Guillaume K!

    Problem solved!

    1. Use ARM Compiler version 5
    2. Use MicroLIB
    3. Uncheck Browse Information
    However, if I want to use ARM Compiler version 6, is there another way?

    Thanks you, Guillaume K!

    ST Employee
    November 19, 2024

    @TonyRuan wrote:

     

    4. Compiling with the option [ARM Compiler: Use default compiler version 5] results in an unusually very slow compilation time.

    On MDK-ARM compiler 5 , it is the generation of code browsing information that takes time. To disable it, you can uncheck "Browse information" in Output tab of your project config.