Skip to main content
Graduate
December 28, 2025
Solved

Ethern Config and ping test

  • December 28, 2025
  • 1 reply
  • 113 views

Good morning, I've been trying to create a simple program for several days that allows me to ping from my laptop to my Nucle F767ZTI board, but to no avail. I'm using CUBE IDE 1.18. I initially followed a tutorial and was able to do it, but only in debug mode, not with the board in running mode (normal operation), without using FreeRTOS but only by enabling ETH and LWIP. Is there a project I can import and then continue making my subsequent changes from there? This is because the ping is only the initial part of my project that I'm about to create. Can you send me a link where I can download and import the project? Thanks in advance.

Here some lines codes that I use:

 

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : main.c
 * @brief : Main program body
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2025 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
#include "lwip.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */

/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */

/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/

UART_HandleTypeDef huart3;

PCD_HandleTypeDef hpcd_USB_OTG_FS;

/* USER CODE BEGIN PV */

/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MPU_Config(void);
static void MX_GPIO_Init(void);
static void MX_USART3_UART_Init(void);
static void MX_USB_OTG_FS_PCD_Init(void);
/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
extern struct netif gnetif;
/* USER CODE END 0 */

/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{

 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MPU Configuration--------------------------------------------------------*/
 MPU_Config();

 /* Enable the CPU Cache */

 /* Enable I-Cache---------------------------------------------------------*/
 SCB_EnableICache();

 /* Enable D-Cache---------------------------------------------------------*/
 SCB_EnableDCache();

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_USART3_UART_Init();
 MX_USB_OTG_FS_PCD_Init();
 MX_LWIP_Init();
 /* USER CODE BEGIN 2 */

 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
	 ethernetif_input(&gnetif);
	 sys_check_timeouts();
	 HAL_Delay(1);
 }
 /* USER CODE END 3 */
}

/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 /** Configure LSE Drive Capability
 */
 HAL_PWR_EnableBkUpAccess();

 /** Configure the main internal regulator output voltage
 */
 __HAL_RCC_PWR_CLK_ENABLE();
 __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);

 /** Initializes the RCC Oscillators according to the specified parameters
 * in the RCC_OscInitTypeDef structure.
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
 RCC_OscInitStruct.HSEState = RCC_HSE_BYPASS;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
 RCC_OscInitStruct.PLL.PLLM = 4;
 RCC_OscInitStruct.PLL.PLLN = 216;
 RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
 RCC_OscInitStruct.PLL.PLLQ = 9;
 RCC_OscInitStruct.PLL.PLLR = 2;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /** Activate the Over-Drive mode
 */
 if (HAL_PWREx_EnableOverDrive() != HAL_OK)
 {
 Error_Handler();
 }

 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_7) != HAL_OK)
 {
 Error_Handler();
 }
}

/**
 * @brief USART3 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_USART3_UART_Init(void)
{

 /* USER CODE BEGIN USART3_Init 0 */

 /* USER CODE END USART3_Init 0 */

 /* USER CODE BEGIN USART3_Init 1 */

 /* USER CODE END USART3_Init 1 */
 huart3.Instance = USART3;
 huart3.Init.BaudRate = 115200;
 huart3.Init.WordLength = UART_WORDLENGTH_8B;
 huart3.Init.StopBits = UART_STOPBITS_1;
 huart3.Init.Parity = UART_PARITY_NONE;
 huart3.Init.Mode = UART_MODE_TX_RX;
 huart3.Init.HwFlowCtl = UART_HWCONTROL_NONE;
 huart3.Init.OverSampling = UART_OVERSAMPLING_16;
 huart3.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
 huart3.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
 if (HAL_UART_Init(&huart3) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN USART3_Init 2 */

 /* USER CODE END USART3_Init 2 */

}

/**
 * @brief USB_OTG_FS Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_USB_OTG_FS_PCD_Init(void)
{

 /* USER CODE BEGIN USB_OTG_FS_Init 0 */

 /* USER CODE END USB_OTG_FS_Init 0 */

 /* USER CODE BEGIN USB_OTG_FS_Init 1 */

 /* USER CODE END USB_OTG_FS_Init 1 */
 hpcd_USB_OTG_FS.Instance = USB_OTG_FS;
 hpcd_USB_OTG_FS.Init.dev_endpoints = 6;
 hpcd_USB_OTG_FS.Init.speed = PCD_SPEED_FULL;
 hpcd_USB_OTG_FS.Init.dma_enable = DISABLE;
 hpcd_USB_OTG_FS.Init.phy_itface = PCD_PHY_EMBEDDED;
 hpcd_USB_OTG_FS.Init.Sof_enable = DISABLE;
 hpcd_USB_OTG_FS.Init.low_power_enable = DISABLE;
 hpcd_USB_OTG_FS.Init.lpm_enable = DISABLE;
 hpcd_USB_OTG_FS.Init.vbus_sensing_enable = ENABLE;
 hpcd_USB_OTG_FS.Init.use_dedicated_ep1 = DISABLE;
 if (HAL_PCD_Init(&hpcd_USB_OTG_FS) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN USB_OTG_FS_Init 2 */

 /* USER CODE END USB_OTG_FS_Init 2 */

}

/**
 * @brief GPIO Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_GPIO_Init(void)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};
 /* USER CODE BEGIN MX_GPIO_Init_1 */

 /* USER CODE END MX_GPIO_Init_1 */

 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOC_CLK_ENABLE();
 __HAL_RCC_GPIOH_CLK_ENABLE();
 __HAL_RCC_GPIOA_CLK_ENABLE();
 __HAL_RCC_GPIOB_CLK_ENABLE();
 __HAL_RCC_GPIOD_CLK_ENABLE();
 __HAL_RCC_GPIOG_CLK_ENABLE();

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(GPIOB, LD3_Pin|LD2_Pin, GPIO_PIN_RESET);

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(USB_PowerSwitchOn_GPIO_Port, USB_PowerSwitchOn_Pin, GPIO_PIN_RESET);

 /*Configure GPIO pins : LD3_Pin LD2_Pin */
 GPIO_InitStruct.Pin = LD3_Pin|LD2_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

 /*Configure GPIO pin : USB_PowerSwitchOn_Pin */
 GPIO_InitStruct.Pin = USB_PowerSwitchOn_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(USB_PowerSwitchOn_GPIO_Port, &GPIO_InitStruct);

 /*Configure GPIO pin : USB_OverCurrent_Pin */
 GPIO_InitStruct.Pin = USB_OverCurrent_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(USB_OverCurrent_GPIO_Port, &GPIO_InitStruct);

 /* USER CODE BEGIN MX_GPIO_Init_2 */

 /* USER CODE END MX_GPIO_Init_2 */
}

/* USER CODE BEGIN 4 */

/* USER CODE END 4 */

 /* MPU Configuration */

void MPU_Config(void)
{

 /* Disables the MPU */
 HAL_MPU_Disable();

 /* Enables the MPU */
 HAL_MPU_Enable(MPU_PRIVILEGED_DEFAULT);

}

/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */
 __disable_irq();
 while (1)
 {
 }
 /* USER CODE END Error_Handler_Debug */
}

#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * @PAram file: pointer to the source file name
 * @PAram line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */

tks

 

    This topic has been closed for replies.
    Best answer by STackPointer64

    Hello @SMusc.1,

    I suggest you follow this article, skip the FreeRTOS sections, and keep the packet polling as you did in the while loop.

    The most important parts are MPU configuration and proper memory configuration. Please make sure you follow these carefully and get back to me.

    Best regards,

    1 reply

    Technical Moderator
    December 29, 2025

    Hello @SMusc.1,

    I suggest you follow this article, skip the FreeRTOS sections, and keep the packet polling as you did in the while loop.

    The most important parts are MPU configuration and proper memory configuration. Please make sure you follow these carefully and get back to me.

    Best regards,

    SMusc.1Author
    Graduate
    December 29, 2025

    Good morning, I want to thank you so much for the tutorial, which allowed me to get straight to the point and thus be able to ping my Nucleo board. A huge thank you, truly. It's an excellent guide, without which I would never have been able to do it. Have a great day!

    Technical Moderator
    December 29, 2025

    You are most welcome, I'm glad I could help!