ethernet delay between the requenst and response
HELLO,
I'm using the stm32H755zit6 nucleo144 board, and I'm trying to communicate with the PC throw ethernet, all is working fine but the delay between the request and response is not enough for our application it's between 1ms to 0.5ms and we need at least (0.1ms or 0.05ms), I don't know where the code is spending all this time, can anyone help me please?
The code was generated using STM32CubeMX 6.9.0 and STM32CubeIDE 1.14 with the package v1.11.0