Skip to main content
Visitor II
January 17, 2024
Question

Ethernet issue after power cycling of STM32H723ZG

  • January 17, 2024
  • 6 replies
  • 5315 views

I'm having the same problem with STM32H723ZG, with our own board, Ethernet can only be connected after using ST link to download the code (either by "debug" or "run"). After power cycle the board, it won't connect anymore, reset button didn't help.  I tried your change to uncomment out "#define DATA_IN_D2_SRAM"

and it didn't help either. Checking LWIP echo servo example, it also has "#define DATA_IN_D2_SRAM"

commented out but okay to connect after power up with Nucleo STM32H723ZG Eval board. But running the same

example code on our board, it works after download but not after power up.

I'm using Hal driver FW1.11.1.. How do you make memory dump using Cube programmer? The ST link utility doesn't

work with this H7 chip. Anything else I should check?

Thank you.

 

 

 

    This topic has been closed for replies.

    6 replies

    Technical Moderator
    January 24, 2024

    Question moved to a new thread. Initially asked in (Solved) I have an ethernet issue after power cycling of H7 Nucleo board.

    ST Employee
    January 24, 2024

    Hello @ETong.1 ,

    This could be due to some miss-configuration of the MPU causing it to fail at run time it seems like the Ethernet is unable to access its DMA buffer descriptors so i suggest you check the configuration of the MPU and then place the descriptors manually in the D2_SRAM this is explained in details in the following article .if you still facing this issue it will be helpful to know about your configuration and changes to the Linker file .

    BR

     

    ETong.1Author
    Visitor II
    January 25, 2024

    Hi @STea ,

    Thanks for your reply.  

    What I changed was RMII pins from low speed to very high.  After that, right after power cycle the board, pressing reset can get Ethernet connection. Then we made hardware change to add a delay to the reset circuit.  Now power cycle the board works too.  I'm not totally convinced that this is the root cause.  You would think pin speed may affect the connection performance but should still allow connection, right?

    Here are the configurations of our system:

    Not using RTOS, using lwIP.

    Using external crystal 25mhz, not same as Eval board that from STlink, so RCC select HSE Crystal/Ceramic Resonator instead of BYPASS clock source.

    CPU set as 550mhz.

    MPU setting: flash.ld

    /* Specify the memory areas */

    MEMORY

    {

    ITCMRAM (xrw) : ORIGIN = 0x00000000, LENGTH = 64K

    DTCMRAM (xrw) : ORIGIN = 0x20000000, LENGTH = 128K

    FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 1024K

    RAM_D1 (xrw) : ORIGIN = 0x24000000, LENGTH = 320K

    RAM_D2 (xrw) : ORIGIN = 0x30000000, LENGTH = 32K

    RAM_D3 (xrw) : ORIGIN = 0x38000000, LENGTH = 16K

    }

    Descriptors are in D2_SRAM area

    ETong1_0-1706141300964.png

    What else I could missing?  Any manual changes that I need to make?

     

     

    ST Employee
    January 31, 2024

    Hello @ETong.1 

    answering your question "You would think pin speed may affect the connection performance but should still allow connection, right?" yes this is right .

    also i think you should try to bypass the delayed reset circuit and see the affect on the behavior because i think this delayed reset can lead to miss-configuration of the PHY interface . this is just a recommendation because after checking your software setup and configuration i think this problem is related to your hardware design . it would help if you could send us a snapshot of your design to analyse it .

    BR

    ETong.1Author
    Visitor II
    January 31, 2024

    Hi BR,

    Here are two changes made in the hardware:

    one was PDR_ON signal Pin 143 had two resistors R138 10k to VDD and R139 10k to ground. Change made to remove R139 to ground.

    Before

    ETong1_0-1706740548122.png

    After

    ETong1_1-1706740564007.png

    2nd change was to add the delay to the RST pin to keep it stay grounded for 68ms upon power up.

    Before change:

    ETong1_2-1706740622095.png

    After change

    ETong1_3-1706740739425.png

    ETong1_4-1706740742481.png

    Let me know what you think.  Appreciate your help.

     

     

    ST Employee
    February 1, 2024

    Hello @ETong.1 ,

    1. can you confirm that the modification to the RST circuit inserted the 68ms you which to have if you can send the snapshot of the scope showing the behavior of the RST ?
    2. why did you remove the resistor connecting the PDR_on to the ground ?is there a practical reason behind this change ?

    Best Regards

    ETong.1Author
    Visitor II
    February 1, 2024

    Hi @STea ,

    1. Here is the scope shot of RST:

    ETong1_0-1706820476984.png

    On the scope ch1 shows the 5v signal with no delay. Ch2 shows the 3.3v signal which is delayed and used to hold the NRST pin Low for that time. (~68ms theoretical, measured ~80ms).

    2. Hardware designer found it from this ST application note:

    https://www.st.com/resource/en/application_note/an5419-getting-started-with-stm32h723733-stm32h725735-and-stm32h730-value-line-hardware-development-stmicroelectronics.pdf

    For packages embedding the PDR_ON pin, the power supply supervisor is enabled by holding PDR_ON high. Thus, the resistor connecting PDR_ON to ground was removed.

    ETong1_1-1706820591866.png

    Thanks

    ST Employee
    February 12, 2024

    Hello @ETong.1 ,

    Do you have any update on the issue that you are facing because it seems like it's not related to software or drivers did you check for resistor values capacitors if there is a solder bridge used on the nucleo board that you are missing in your implementation. i'm looking forward to know the root cause of this problem .

    BR

    ETong.1Author
    Visitor II
    February 23, 2024

    Hi @STea ,

    So far we're using the above two changes I mentioned made to the board as the solution. 

    Have you looked at the scope shot and ST app note and see if our changes are correct?

    Thanks