Ethernet + LwIP + FreeRTOS Issues on NUCLEO-H753ZI
Hi guys,
I have a STM32 NUCLEO-H753ZI board and the overall goal is to run open62541. In order to do that, I need a working LwIP stack and Ethernet connection. I have done a lot of research and tried multiple settings, but can´t get it working. Below, I´ll describe what I have done so far / settings in the .ioc I have made.
It would be awesome if you could tell me, where my mistake is.
Using STM32CubeIDE Version: 1.19.0 Build: 25607_20250703_0907 (UTC).
Clock Configuration:
Input frequency = 8MHz -> PLL Source Mux = HSE -> System Clock Mux = PLLCLK (Enable CSS)
-> SYSCLOCK = 400 MHz -> D1 CPRE Prescaler = /1 -> 400 MHz -> HPRE Prescaler = /2 -> 200 MHz
-> D1 PPRE, D2 PPRE1, D2 PPRE2, D3 PPRE = /2
System Core:
RCC:
HSE = BYPASS Clock Source
LSE = Crystal
Power Regulator Voltage Scale = Power Regulator Voltage Scale 1
SYS:
Timebase Source = TIM6
NVIC:
Ethernet global interrupt = Enabled, Preemption Priority = 5
Ethernet wake-up interrupt through EXTI line 86 = Enabled, Preemption Priority = 5
CORTEX_M7:
See Screenshot attached below.
Connectivity:
ETH:
Enabled in RMII
NVIC Settings as described in NVIC
GPIO Settings: Set Maximum output speed to "Very High" for every Pin
Middleware and Software Packs:
FreeRTOS:
Using CMSIS v1 (FreeRTOS version 10.3.1, CMSIS-RTOS version 1.02)
ENABLE_FPU = Enabled
MINIMAL_STACK_SIZE = 1024 Words
TOTAL_HEAP_SIZE = 300000 Bytes
Memory Management scheme = heap_4
LWIP:
Platform Settings: LAN8742 and as Solution also LAN8742
General Settings: DHCP = Disabled, Set own IP-Address, Netmask and Gateway (those are fine)
General Settings: ICMP, DNS, UDP, TPC = Enabled
Key Options: Please see .pdf with Screenshots below
Preprocessor:
Under Properties -> C/C++ Build -> MCU/MPU GCC Compiler -> Preprocessor I added "DATA_IN_D2_SRAM"
to the Define symbols.
_FLASH.id:
/* Specify the memory areas */
MEMORY
{
FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 2048K
DTCMRAM (xrw) : ORIGIN = 0x20000000, LENGTH = 128K
RAM_D1 (xrw) : ORIGIN = 0x24000000, LENGTH = 512K
RAM_D2 (xrw) : ORIGIN = 0x30020000, LENGTH = 256K /* SRAM2 */
RAM_D2_SRAM3 (xrw) : ORIGIN = 0x30040000, LENGTH = 32K /* SRAM3 */
RAM_D3 (xrw) : ORIGIN = 0x38000000, LENGTH = 64K
ITCMRAM (xrw) : ORIGIN = 0x00000000, LENGTH = 64K
}And between .data and .bss I added:
/* --- Ethernet DMA descriptors -> D2 SRAM3 --- */
ETH_DESCRIPTORS (NOLOAD) :
{
. = ALIGN(32);
*(.RxDecripSection)
*(.TxDecripSection)
. = ALIGN(32);
} >RAM_D2_SRAM3
/* --- Ethernet buffers -> D2 SRAM2 --- */
ETH_BUFFERS (NOLOAD) :
{
. = ALIGN(32);
*(.Rx_PoolSection)
*(.RxArraySection)
*(.TxArraySection)
. = ALIGN(32);
} >RAM_D2And in ethernetif.c there is:
#if defined ( __ICCARM__ ) /*!< IAR Compiler */
#pragma location = 0x30000100
extern u8_t memp_memory_RX_POOL_base[];
#elif defined ( __CC_ARM ) /* MDK ARM Compiler */
__attribute__((section(".Rx_PoolSection"))) extern u8_t memp_memory_RX_POOL_base[];
#elif defined ( __GNUC__ ) /* GNU */
__attribute__((section(".Rx_PoolSection"))) extern u8_t memp_memory_RX_POOL_base[];
#endifin the .map there is:
ETH_DESCRIPTORS
0x30040000 0xc0
0x30040000 . = ALIGN (0x20)
*(.RxDecripSection)
.RxDecripSection
0x30040000 0x60 ./LWIP/Target/ethernetif.o
0x30040000 DMARxDscrTab
*(.TxDecripSection)
.TxDecripSection
0x30040060 0x60 ./LWIP/Target/ethernetif.o
0x30040060 DMATxDscrTab
0x300400c0 . = ALIGN (0x20)
ETH_BUFFERS 0x30020000 0x6220
0x30020000 . = ALIGN (0x20)
*(.Rx_PoolSection)
.Rx_PoolSection
0x30020000 0x6203 ./LWIP/Target/ethernetif.o
0x30020000 memp_memory_RX_POOL_base
*(.RxArraySection)
*(.TxArraySection)
0x30026220 . = ALIGN (0x20)
When debugging, it always ends in an endless loop somewhere or jumps to a Hard Fault.
Couldn`t really figure out why or which specific error it is.
If you have any tips or maybe some kind of example project where LwIP + FreeRTOS is working, that would be awesome.
Cheers,
Gregor