Ethernet MAC and its DMA controller is not getting reset in STM32H733xx MCU
I am using STM32H733ZGT6 in my project. For Ethernet communication, KSZ8081RNB PHY is configured in 25MHz mode such that PHY has to supply the 50MHz clock to MAC in my MCU. Problem here is, when I try to reset the MAC and its DMA controller by setting the 0th bit in ETH_DMAMR register, Reset operation is not completing (0th bit is still set by Hardware). I found that PHY's reference clock (50Hz) is not obtained, Is this the only reason? I am not sure what other conditions I am missing to complete the Reset. Please help me to resolve this.