Skip to main content
Visitor II
April 9, 2021
Question

Ethernet Rx FIFO Overflow - Reported number of dropped frames inconsistent, interrupt appears deffered

  • April 9, 2021
  • 0 replies
  • 730 views

Hello,

As part of my internship, I am tasked with writing a device driver for the Ethernet programmable interface. I am currently trying to understand the behaviour of the interface under receive overflow conditions.

2 things puzzle me:

  • The cumulated number of discarded frames caused by Rx queue overflows is HIGHER than the number of frames I actually do not receive on the application side. I compute the number of frames lost in overflows by regularly incrementing an internal counter with the value in ETH_MTLRXQMPOCR.OVFPKTCNT. As the ETH_MTLRXQMPOCR.OVFPKTCNT resets itself each time the register is read, I believe this should not be the cause of my issue. As for the number of actually lost frames, I am in control of the frames I send to the interface, and just set an increasing number as their payload (1st frame carries idx = 1, 2nd frame carries idx = 2, etc.), which I then use to figure out which frames are missing on the receive side.
  • The "Rx queue overflow" interrupt gets triggered a long time the ETH_MTLRXQMPOCR.OVFPKTCNT overflow counter becomes > 0, or after I actually start seeing dropped frames on the application side. I am talking enough time to receive dozens of frames and "Receive complete" interrupts.

I'm afraid I fundamentally misunderstand how the interface handles receive overflows. Is this expected behaviour?

Thanks.

    This topic has been closed for replies.