Skip to main content
Visitor II
January 29, 2021
Question

Execution control will always be at HAL_I2C_Master_Receive() function while reading the data from RMCS220x DC Servo Motor

  • January 29, 2021
  • 0 replies
  • 689 views

Hi,

I am writing an application with STM32F746g Discovery board where i need to get the data from the RMCS-220X based Encoder DC Servo Motor with I2C interface.

I have written the driver code based on the Arduino Library. Arduino code is working perfectly while reading /writing the data from the Motor with I2C bus.

With the modified code based on HAL Libraries, I am able to write the data to the motor but unable to read the data from Motor because execution always stuck at "while(HAL_I2C_Master_Receive(&hi2c1, I2C_ADDRESS, data, 2, 1000) != HAL_OK);" this line.

Board: STM32F746G Discovery

CubeF7 Firmware Version: 1.16.0

I2C Clock: 100KHz

Could you please let me know how to proceed and needful.

    This topic has been closed for replies.