Skip to main content
Visitor II
May 25, 2020
Question

External IP connection failure

  • May 25, 2020
  • 0 replies
  • 546 views

I am working on STM32F407, with Ethernet chip DP83848 PHY, None Os, LwIP

I tested the source below with an example.

STM32Cube_FW_F4_V1.24.0\Projects\STM324x9I_EVAL\Applications\LwIP\LwIP_TCP_Echo_Client

Internal IP connection is good. Ex) IP : 192.168.0.200 Subnet Mask: 255.255.225.0 GateWay: 192.168.0.1 

No external IP connection. Ex) IP : 119.65.244.256 PORT: 10000

I can't get out of the source below

ip4_route(const ip4_addr_t *dest)

{

 struct netif *netif;

 ..SKIP

 /* iterate through netifs */

 for (netif = netif_list; netif != NULL; netif = netif->next) {

   /* is the netif up, does it have a link and a valid address? */

   if (netif_is_up(netif) && netif_is_link_up(netif) && !ip4_addr_isany_val(*netif_ip4_addr(netif))) {

     /* network mask matches? */

     if (ip4_addr_netcmp(dest, netif_ip4_addr(netif), netif_ip4_netmask(netif))) {

       /* return netif on which to forward IP packet */

       return netif;

     }

     /* gateway matches on a non broadcast interface? (i.e. peer in a point to point interface) */

     if (((netif->flags & NETIF_FLAG_BROADCAST) == 0) && ip4_addr_cmp(dest, netif_ip4_gw(netif))) {

       /* return netif on which to forward IP packet */

       return netif;

     }

   }

 }

 .. SKIP

}

Need help

    This topic has been closed for replies.