Extracting an existing hex to edit in CubeIDE
Hello,
Right now I am working on a Riverdi display, actually the RVT101HVSNWC00-B.
I was able to connect with their external loader and to save the firmware in Bin and Hex formats. I wanted to review the firmware, as loaded, in CubeIDE.
How would I do that without having to go through the trouble of setting up the board/ peripherals and pins? I want to review and edit what is on the board. Most of what I would need to set the peripherals and pins is in the code.
I have read through all sorts of documentation and there is no direct path that I have been able to find. Any assistance would be appreciated.
I can't seem to add the hex file because of the following...
(application/octet-stream) does not match its file extension
Thanks