Skip to main content
Visitor II
November 2, 2024
Solved

F410: multiple definition of `huart2';

  • November 2, 2024
  • 2 replies
  • 1282 views

HI there, i m using F410 Nucleo, and i keep getting these errors when using USART2, as I declare in 2 separe files i.e. main.c and buffer.  could anyone advise how to resolve this?

error: multiple definition of `huart2';

 

//main.c
..
/* Private variables ---------------------------------------------------------*/
UART_HandleTypeDef huart2;
..
 /* USER CODE END USART2_Init 1 */
 huart2.Instance = USART2;
 huart2.Init.BaudRate = 115200;
 huart2.Init.WordLength = UART_WORDLENGTH_8B;
 huart2.Init.StopBits = UART_STOPBITS_1;
 huart2.Init.Parity = UART_PARITY_NONE;
 huart2.Init.Mode = UART_MODE_TX_RX;
 huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;
 huart2.Init.OverSampling = UART_OVERSAMPLING_16;



// buffer.c
#include "buffer.h"
#include <string.h>
/**** define the UART ****/
UART_HandleTypeDef huart2; // woldes
#define uart &huart2
..

 

 

 

    This topic has been closed for replies.
    Best answer by gbm

    Your question is about basics of C programming; it's not related to STM32.The whole program may contain only a single definition of a symbol. Define the huart2 in one module only (maybe buffer.c - it's already defined there), put its declaration as extern in buffer.h:

    extern UART_HandleTypeDef huart2;

    Include buffer.h in main.c.

    2 replies

    gbmAnswer
    Graduate
    November 2, 2024

    Your question is about basics of C programming; it's not related to STM32.The whole program may contain only a single definition of a symbol. Define the huart2 in one module only (maybe buffer.c - it's already defined there), put its declaration as extern in buffer.h:

    extern UART_HandleTypeDef huart2;

    Include buffer.h in main.c.

    Super User
    November 2, 2024

    @gbm wrote:

    Include buffer.h in main.c.


    Indeed.

    @HMSEdinburge  Also Include buffer.h in buffer.c - that way the compiler gets to check that they are  consistent:

    https://community.st.com/t5/stm32cubeide-mcus/adding-new-c-source-files-to-my-project-and-navigating-through/m-p/658310/highlight/true#M25925

    Super User
    November 2, 2024

    As @gbm said, this is standard C stuff - nothing specific to STM32.

     


    @HMSEdinburge wrote:

     as I declare (sic) in 2 separe files i.e. main.c and buffer. 


    No, you are defining in both files - that's why the compilers says, "multiple definitions"!

     

    This is a definition - the comment even says it:

    /**** define the UART ****/
    UART_HandleTypeDef huart2; // woldes

    and this is also a definition:

    /* Private variables ---------------------------------------------------------*/
    UART_HandleTypeDef huart2;

    So that is multiple definitions!

    Note that the comment saying "Private variables" is incorrect:  to make that variable private, you would need to make it static, but then it would be distinct from the huart2 in the other file - they would not be the same variable.

     

    See this post for how to properly share variables (and functions) between files in C:

    https://community.st.com/t5/stm32cubeide-mcus/adding-new-c-source-files-to-my-project-and-navigating-through/m-p/657455/highlight/true#M25847