Fast ADC transfer and accumulate to on array - STM32U595
Hi ST community,
I'm struggling to get required transfer and accumulate rate from ADC to an array, I'm focusing at the moment to the data transfer phase, which seems the slowest one.
Situation:
using STMCube IDE Version: 1.14.0
using 3 ADC: ADC1 ADC2 ADC4 to simultaneously acquire 3 signals, ADC start conversion is triggered by timer event.
Transfer of data is in the form of array[idx] = array[idx] + ADCdata in the HAL_ADC_ConvCpltCallback callback. When ADCx_seqPhase == 0, ADC data is transfered directly ( zeroing phase ).
Array indexes are managed outside of this function.
code is
void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef *hadc)
{
if(hadc->Instance == ADC1)
{
if (ADC1_seqPhase == 0)
{
S.array[ altArrayACQ_ADC1 ][Array_Pointer-1] = ADC1->DR;
}
else
{
S.array[ altArrayACQ_ADC1 ][Array_Pointer-1] += ADC1->DR;
}
}
if(hadc->Instance == ADC2)
{
if (ADC1_seqPhase == 0)
{
S.array[ altArrayACQ_ADC2 ][Array_Pointer-1] = ADC2->DR;
}
else
{
S.array[ altArrayACQ_ADC2 ][Array_Pointer-1] += ADC2->DR;
}
}
if(hadc->Instance == ADC4)
{
if (ADC1_seqPhase == 0)
{
S.array[ altArrayACQ_ADC4 ][Array_Pointer-1] = ADC4->DR;
}
else
{
S.array[ altArrayACQ_ADC4 ][Array_Pointer-1] += ADC4->DR;
}
}
}
Looking at the compiled list ( only for the ADC1, just to avoid rewriting the same code 3 times) I see lots of low level instructions, which can somehow explain why performance is quite low.
if (ADC1_seqPhase == 0)
8003c66: 4b56 ldr r3, [pc, #344] ; (8003dc0 <HAL_ADC_ConvCpltCallback+0x16c>)
8003c68: 781b ldrb r3, [r3, #0]
8003c6a: 2b00 cmp r3, #0
8003c6c: d110 bne.n 8003c90 <HAL_ADC_ConvCpltCallback+0x3c>
{
S.array[ altArrayACQ_ADC1 ][Array_Pointer-1] = ADC1->DR;
8003c6e: 4a53 ldr r2, [pc, #332] ; (8003dbc <HAL_ADC_ConvCpltCallback+0x168>)
8003c70: 4b54 ldr r3, [pc, #336] ; (8003dc4 <HAL_ADC_ConvCpltCallback+0x170>)
8003c72: 781b ldrb r3, [r3, #0]
8003c74: 461c mov r4, r3
8003c76: 4b54 ldr r3, [pc, #336] ; (8003dc8 <HAL_ADC_ConvCpltCallback+0x174>)
8003c78: 881b ldrh r3, [r3, #0]
8003c7a: 3b01 subs r3, #1
8003c7c: 6c12 ldr r2, [r2, #64] ; 0x40
8003c7e: 4853 ldr r0, [pc, #332] ; (8003dcc <HAL_ADC_ConvCpltCallback+0x178>)
8003c80: f44f 7196 mov.w r1, #300 ; 0x12c
8003c84: fb04 f101 mul.w r1, r4, r1
8003c88: 440b add r3, r1
8003c8a: f840 2023 str.w r2, [r0, r3, lsl #2]
8003c8e: e01e b.n 8003cce <HAL_ADC_ConvCpltCallback+0x7a>
}
else
{
S.array[ altArrayACQ_ADC1 ][Array_Pointer-1] += ADC1->DR;
8003c90: 4b4a ldr r3, [pc, #296] ; (8003dbc <HAL_ADC_ConvCpltCallback+0x168>)
8003c92: 6c19 ldr r1, [r3, #64] ; 0x40
8003c94: 4b4b ldr r3, [pc, #300] ; (8003dc4 <HAL_ADC_ConvCpltCallback+0x170>)
8003c96: 781b ldrb r3, [r3, #0]
8003c98: 461c mov r4, r3
8003c9a: 4b4b ldr r3, [pc, #300] ; (8003dc8 <HAL_ADC_ConvCpltCallback+0x174>)
8003c9c: 881b ldrh r3, [r3, #0]
8003c9e: 3b01 subs r3, #1
8003ca0: 484a ldr r0, [pc, #296] ; (8003dcc <HAL_ADC_ConvCpltCallback+0x178>)
8003ca2: f44f 7296 mov.w r2, #300 ; 0x12c
8003ca6: fb04 f202 mul.w r2, r4, r2
8003caa: 4413 add r3, r2
8003cac: f850 2023 ldr.w r2, [r0, r3, lsl #2]
8003cb0: 4b44 ldr r3, [pc, #272] ; (8003dc4 <HAL_ADC_ConvCpltCallback+0x170>)
8003cb2: 781b ldrb r3, [r3, #0]
8003cb4: 461c mov r4, r3
8003cb6: 4b44 ldr r3, [pc, #272] ; (8003dc8 <HAL_ADC_ConvCpltCallback+0x174>)
8003cb8: 881b ldrh r3, [r3, #0]
8003cba: 3b01 subs r3, #1
8003cbc: 440a add r2, r1
8003cbe: 4843 ldr r0, [pc, #268] ; (8003dcc <HAL_ADC_ConvCpltCallback+0x178>)
8003cc0: f44f 7196 mov.w r1, #300 ; 0x12c
8003cc4: fb04 f101 mul.w r1, r4, r1
8003cc8: 440b add r3, r1
8003cca: f840 2023 str.w r2, [r0, r3, lsl #2]
}
is there a more clever way to obtain a faster transfer and accumulate of ADC values? I've looked at DMA, but as far as I've understood no accumulate feature is available.
Best regards,
Anton