FATFS not working when if FreeRTOS is enabled
Hello, I've a STM32 NUCLEO board (STM32F446RETx) with an SD card board connected to it.
Im using:
- STM32CubeIDE Version: 1.7.0 Build: 10852_20210715_0634 (UTC)
- STMicroelectronics STM32CubeMX 6.3.0.202107141111 com.st.stm32cube.common.mx
- STM32CubeF4 Firmware Package V1.26.0 / 12-February-2021
SDIO peripheral has been configured properly (DMA for both RX and TX).
I'm executing the following code:
When executed, this code works well and generate both the directory and the file on the SD card as long as FreeRTOS is disable.
If FreeRTOS is enabled " if(f_mount(&fileSystem, "/", 1) == FR_OK)" always fails.
Any known reason for this ? Is there anything that must be done (FreRTOS or FATFS configuration) to make these two modules coexisting ?
Thanks, Joel