FatFs_USBDisk example with USB_FS does not work. When an USB Stick is connected the USBH_MSC_Process never gets further then MSC_READ_INQUIRY. Any hints?
I am trying to implement an USB logger. I have initially started with the F769 Discovery Board what worked fine using the USB_HS implementation. Because my final hardware does use USB_FS and I do not own an F769 Eval Board I tried the FatFs_USBDisk example for the 767 Nucleo board what sows the behavior above.
The Nucleoboard is unmodified, SB 125, 127, 132, 133, !184, 185 set as stated in UM1974. UsbStick and MicroAdapter Tested in HS Example. Example is based on V1.17.0