FileX help
Platform Nucleo-H563ZI
CubeIDE V1.15.0
ioc file attached
I'm starting with a simple app to get fimilar with the new Middleware.
I created a new STM32 app and enabled ThreadX and FileX.
I also changed the recommended settings for IChache and the system timer (TIM2)
I enabled the BSP LEDs, button, and virtual serial port.
For ThreadX I enabled the core and used static allocation
I tried a pool size of 2048 and 8096 with the same results
For FileX I enabled the core and checked the 'Internal RAM Interface' setting
I tried SRAM3 and SRAM1 with the same results
I created one user thread and put the following in it.
while(1)
{
tx_thread_sleep(10);
BSP_LED_Toggle(LED_GREEN);
BSP_LED_Toggle(LED_YELLOW);
BSP_LED_Toggle(LED_RED);
}
The first thing I noticed is that the BSP init code is placed after
MX_ThreadX_Init(), and does not get executed.
I copied that code before MX_ThreadX_Init()
If the call to create the FileX thread in tx_application_define() is executed,
the code crashes with the cursor at the top of _fx_utility_logical_sector_read()
which is called from _fx_utility_FAT_entry_read()
If I comment the line: status = MX_FileX_Init(memory_ptr); and the return check code,
the code runs and my LEDs blink.
Is there something I missed?
Karl