FileX LevelX
I am having trouble integrating LevelX into FileX using the on board eMMC on the STM32H745I-DiSCO eval board. I am using standalone mode (no AzureRTOS). I have successfully implemented FileX to format, write and read the eMMC card in standalone. I am having trouble now integrating LevelX using the IOC file as a basis to generate code. When I try to format the eMMC card with the following call, it returns a status of 144.
status = fx_media_format(&mmc_disk, fx_stm32_levelx_nand_driver, /* Driver entry */
// (VOID *)CUSTOM_DRIVER_ID,
(VOID*) 0xEEEE, mmc_memory, /* Media buffer pointer */
sizeof(mmc_memory), /* Media buffer size */
"EMMC_DISK", /* Volume Name */
FX_EMMC_NUMBER_OF_FATS, /* Number of FATs */
FX_EMMC_DIRECTORY_ENTRIES, /* Directory Entries */
FX_EMMC_HIDDEN_SECTORS, /* Hidden sectors */
FX_EMMC_TOTAL_SECTORS, /* Total sectors */
FX_EMMC_SECTOR_SIZE, /* Sector size */
FX_EMMC_SECTORS_PER_CLUSTER, /* Sectors per cluster */
FX_EMMC_HEADS, /* Heads */
FX_EMMC_SECTORS_PER_TRACK); /* Sectors per track */
The only difference between FileX only code that works and FileX/LevelX code that doesn't is the argument "fx_stm32_levelx_nand_driver" which I believe is required based on another Eval board's example.
When using only FileX, the argument is fx_stm32_mmc_driver. I didn't notice any calls to LevelX low level drivers in fx_stm32_mmc_driver. Any help is appreciated !!!
THANKS!!!