FileX / LevelX / QSPI cannot get the filesystem to startup.
Hello,
Is there any documentation or example on how to setup a STMH7(43) with QSPI and FileX and LevelX? There must be something that is not setup properly. I looked at the Fx_Nor_Write_Read_File project for the STM32H735, but the code and CubeMX settings are completely different from the new project I started with CubeMX.
On my custom board, the system comes up. It starts by calling FX_Media_Format, which calls 'FlashErase; it thinks it successfully erased the entire flash (but I have my doubts), it then sets up the semaphores, and start the actual formatting. lx_stm32_qspi_read() runs 3 times and then fails. I would have expect to see "FFFFFFFF"s on all the reads, but it seems to be getting different data.
I dropped the clock to 50MHz for this test, but it is unclear if the 1/2 clock shift should be enabled or not, and what should the DMA settings be in CubeMX. It seems to be reading the Device ID and passes that test. Is it a memory cache issue?
Any help or suggestions would be helpful
thanks
Matthew
QSPI device is MT25QL256 (32Mbyte)