FLASH_WaitForLastOperation() returning HAL_ERROR
Hi.. I am using STM32L476 Nucleo board.
When i tried to erase a flash page using HAL_FLASHEx_Erase(), the FLASH_WaitForLastOperation() returns a HAL_ERROR
I've seen similar issues in the community, but unfortunately, similar solutions just don't work.
And the error code is 0xA0 , how can I fix this
StatusDef FlashWr(uint32_t flash_addr, uint8_t *pData, uint16_t length)
{
uint8_t *pBuf = (unsigned char *)flash_write_buf;
uint16_t cnt; // valid length in current sector
uint32_t flash_addr_base;
uint32_t addr_offset;
bool cmp_result;
uint16_t i;
uint64_t val;
uint16_t addr;
StatusDef sta = STA_OK;
while (length > 0)
{
flash_addr_base = (uint32_t)(flash_addr & ~FLASH_SECTOR_MASK);
addr_offset = (uint32_t)(flash_addr & FLASH_SECTOR_MASK);
cnt = FLASH_SECTOR_SIZE - addr_offset;
if (length < cnt)
{
cnt = length;
}
FlashRd(flash_addr_base, pBuf, FLASH_SECTOR_SIZE);
cmp_result = FlashCmp(pBuf + addr_offset, pData, cnt);
if (false == cmp_result)
{
if (STA_OK != FlashPageErase(flash_addr_base))
{
return STA_ERROR;
}
Utils_MemCpy(pBuf + addr_offset, pData, cnt); // update the buffer
// program the whole sector
HAL_FLASH_Unlock();
for (i = 0; i < FLASH_BUF_SIZE_64B; i++)
{
val = flash_write_buf[i];
addr = flash_addr_base + i * 8;
sta |= FlashPrg64bit(addr, val);
}
HAL_FLASH_Lock();
}
// next sector
flash_addr += cnt;
pData += cnt;
length -= cnt;
}
return sta;
}StatusDef FlashPageErase(uint32_t addr)
{
StatusDef sta = STA_OK;
uint32_t page_err;
FLASH_EraseInitTypeDef EraseInitStruct = {0};
uint32_t page_idx = (addr - FLASH_BASE) >> 11;
if (FLASH_PAGE_NUM == 256)
{
if (page_idx > 256)
{
return STA_ERROR;
}
if (page_idx > 127)
{
page_idx = page_idx + 128;
}
}
uint32_t banks_idx = page_idx < 256 ? FLASH_BANK_1 : FLASH_BANK_2;
EraseInitStruct.TypeErase = FLASH_TYPEERASE_PAGES;
EraseInitStruct.Banks = banks_idx;
EraseInitStruct.Page = page_idx;
EraseInitStruct.NbPages = 1;
HAL_FLASH_Unlock();
if (HAL_FLASHEx_Erase(&EraseInitStruct, (uint32_t *)&page_err) != 0x00)
{
sta = STA_ERROR;
}
HAL_FLASH_Lock();
return sta;
}