Skip to main content
Visitor II
February 1, 2025
Question

FMC Writing to all Subsequent Memory Addresses

  • February 1, 2025
  • 1 reply
  • 689 views

Hello,

I am trying to use FMC on an STM32U5G9J-DK2 to communicate with an LCD (ST7789). I am trying to send initialization commands to the device as follows

 

define FMC_BANK1_REG ((volatile uint16_t *)0x60000000)
#define FMC_BANK1_DATA ((volatile uint16_t *)0x60000002)

void write_command(uint8_t data)
{
 volatile uint16_t *p = FMC_BANK1_REG;
 *p = (uint16_t)(data);
}

void write_data(uint16_t data)
{
 volatile uint16_t *p = FMC_BANK1_DATA;
 *p = data;
}

// Ex:
write_command(0xFF)

However, when I write 0xFF to memory at address 0x60000000, I don't just see the value written to the single memory address. Instead, it appears to be writing to many subsequent memory addresses. What I see is FF00FF00 written to all addresses between 0x60000000 and 0x600001CC. I understand that the memory is little endian, so FF00 is expected. However, I am unsure why it is repeating to other addresses. I am using the default, CubeMX generated code for FMC initialization, shown below.

/* FMC initialization function */
static void MX_FMC_Init(void)
{

 /* USER CODE BEGIN FMC_Init 0 */

 /* USER CODE END FMC_Init 0 */

 FMC_NORSRAM_TimingTypeDef Timing = {0};

 /* USER CODE BEGIN FMC_Init 1 */

 /* USER CODE END FMC_Init 1 */

 /** Perform the SRAM1 memory initialization sequence
 */
 hsram1.Instance = FMC_NORSRAM_DEVICE;
 hsram1.Extended = FMC_NORSRAM_EXTENDED_DEVICE;
 /* hsram1.Init */
 hsram1.Init.NSBank = FMC_NORSRAM_BANK1;
 hsram1.Init.DataAddressMux = FMC_DATA_ADDRESS_MUX_DISABLE;
 hsram1.Init.MemoryType = FMC_MEMORY_TYPE_SRAM;
 hsram1.Init.MemoryDataWidth = FMC_NORSRAM_MEM_BUS_WIDTH_16;
 hsram1.Init.BurstAccessMode = FMC_BURST_ACCESS_MODE_DISABLE;
 hsram1.Init.WaitSignalPolarity = FMC_WAIT_SIGNAL_POLARITY_LOW;
 hsram1.Init.WaitSignalActive = FMC_WAIT_TIMING_BEFORE_WS;
 hsram1.Init.WriteOperation = FMC_WRITE_OPERATION_ENABLE;
 hsram1.Init.WaitSignal = FMC_WAIT_SIGNAL_DISABLE;
 hsram1.Init.ExtendedMode = FMC_EXTENDED_MODE_DISABLE;
 hsram1.Init.AsynchronousWait = FMC_ASYNCHRONOUS_WAIT_DISABLE;
 hsram1.Init.WriteBurst = FMC_WRITE_BURST_DISABLE;
 hsram1.Init.ContinuousClock = FMC_CONTINUOUS_CLOCK_SYNC_ONLY;
 hsram1.Init.WriteFifo = FMC_WRITE_FIFO_ENABLE;
 hsram1.Init.NBLSetupTime = 0;
 hsram1.Init.PageSize = FMC_PAGE_SIZE_NONE;
 hsram1.Init.MaxChipSelectPulse = DISABLE;
 /* Timing */
 Timing.AddressSetupTime = 3;
 Timing.AddressHoldTime = 15;
 Timing.DataSetupTime = 2;
 Timing.DataHoldTime = 2;
 Timing.BusTurnAroundDuration = 2;
 Timing.CLKDivision = 16;
 Timing.DataLatency = 17;
 Timing.AccessMode = FMC_ACCESS_MODE_A;
 /* ExtTiming */

 if (HAL_SRAM_Init(&hsram1, &Timing, NULL) != HAL_OK)
 {
 Error_Handler();
 }

 /* USER CODE BEGIN FMC_Init 2 */

 /* USER CODE END FMC_Init 2 */
}

 

If anyone could provide help on this matter, it would be greatly appreciated.

    This topic has been closed for replies.

    1 reply

    Graduate II
    February 2, 2025

    What's the screen shot showing? A memory view of FMC.

    You're probably decoding one address bit, so read content is just going to repeat, as that bit goes high and low whilst other undecoded bits go ignored.