Skip to main content
Explorer
June 6, 2024
Solved

FP-SNS-ALLMEMS1 not found in cube ide

  • June 6, 2024
  • 1 reply
  • 797 views

Hi

I am trying to set up a project based on FP-SNS-ALLMEMS1.

When i set up a project based on STM32L476 Nucleo, I cant find the pack neither under "select components" nor under "manage software packs". see below

Why??

MK1_0-1717666159417.png

 

    This topic has been closed for replies.
    Best answer by Peter BENSCH

    Unfortunately, not all software packages are yet integrated in STM32CubeIDE, so that in such cases it is only possible to open or create projects manually. To do this, you can download the firmware FP-SNS-ALLMEMS1, unpack it (for Windows, please use short paths) and open the STM32L476RG-Nucleo projects directly from there, for example.

    Hope that helps?

    Regards
    /Peter

    1 reply

    Technical Moderator
    June 6, 2024

    Unfortunately, not all software packages are yet integrated in STM32CubeIDE, so that in such cases it is only possible to open or create projects manually. To do this, you can download the firmware FP-SNS-ALLMEMS1, unpack it (for Windows, please use short paths) and open the STM32L476RG-Nucleo projects directly from there, for example.

    Hope that helps?

    Regards
    /Peter