FPU_Fractal in STM32CubeH7 Firmware freezes in STM32H747I-DISCO
Hello, hello.
In the STM32CubeH7 Firmware Package V1.12.0 and earlier is a demo application
under Projects/STM32H747I-DISCO/Applications/FPU/FPU_Fractal.
The app waits in an endless loop in line 252:
while(pending_buffer != 0)
{
} A breakpoint in the callback function
void HAL_DSI_EndOfRefreshCallback(DSI_HandleTypeDef *hdsi)
{
...
}is never reached where pending_buffer should be set to 0.
I also flashed CM4 and CM7 code. I did not test every example, some work.
Board version is: MB1248-H747I-D03
Did anyone try this example?