Get Time error on B-L475E-IOT01A_Iot_Node while reset
Hi,
After installing the x-cube-aws demo software, when I turn on the board, the following error occurs.
>>>
.........................
Module initialized successfully: Inventek eS-WiFi ISM43362-M3G-L44-SPI C3.5.2.5.STM
Retrieving the WiFi module MAC address: c4:xx:xx:xx:xx:1f
Connecting to AP: e4ds_studio Attempt 1/3 ...
Connected to AP e4ds_studio
Mac address: c4:xx:xx:xx:xx:xx
Retrieving the IP address.
IP address: 172.xx.x.xx
Push the User button (Blue) within the next 5 seconds if you want to update the device security parameters or credentials.
Setting the RTC from the network time.
ERROR: net_sock_open_mbedtls L#165 failed
! mbedtls_x509_crt_parse returned -0x2180 while parsing root cert
ERROR: setRTCTimeDateFromNetwork L#134 Could not open the socket.
Error initializing the RTC from the network time!