Skip to main content
Visitor II
February 26, 2021
Question

Getting sleep to work when USB CDC is enabled?

  • February 26, 2021
  • 13 replies
  • 3179 views

My program has the option of sleeping for a period using the RTC to wake or sleeping until the wakeup pin is set high. Both these functions work perfectly if I talk to the outside world using a uart.

However, I configure CDC as a serial port SLEEP doesn't work - or at least the USB never disconnects.

I'm using USB STOP and USB DEINIT before the sleep command but these don't seem to do anything. Any ideas appreciated

 while(totalseconds>0){
 if(totalseconds>30.0){
 timetosleep=30*2048;
 totalseconds-=30.0;
 } else {
 timetosleep= (int)(totalseconds*2048.0);
 totalseconds=0.0;
 }
 USBD_Stop(&hUsbDeviceFS);
 USBD_DeInit(&hUsbDeviceFS);
 HAL_NVIC_SetPriority(RTC_WKUP_IRQn, 0x0F, 0);
 HAL_NVIC_EnableIRQ(RTC_WKUP_IRQn);
 HAL_RTCEx_SetWakeUpTimer_IT(&hrtc, timetosleep, RTC_WAKEUPCLOCK_RTCCLK_DIV16);
 HAL_SuspendTick();
 HAL_PWR_EnterSTOPMode(PWR_LOWPOWERREGULATOR_ON, PWR_STOPENTRY_WFE);
 HAL_RTCEx_DeactivateWakeUpTimer(&hrtc);
 HAL_NVIC_DisableIRQ(RTC_WKUP_IRQn);
 }
 SYSCLKConfig_STOP();
 HAL_ResumeTick();
 MX_USB_DEVICE_Init();

    This topic has been closed for replies.

    13 replies

    Visitor II
    February 26, 2021

    Hi PMath.4,

    Can you please provide the product or the MCU family you are working with ?

    Best Regards,

    Ons.

    PMath.4Author
    Visitor II
    February 26, 2021

    Oops - sorry. STM32F407VET

    Super User
    February 26, 2021

    And the hardware? Is this some "known good" board like Nucleo or Disco? Is there any external pullup to DP/DM?

    What exactly means "USB never disconnects"?

    JW

    PMath.4Author
    Visitor II
    February 27, 2021

    Standard wiring using the internal phy with a 22R to the pins and a 1.5K pulldown up on D+ at the USB socket.

    "What exactly means "USB never disconnects"?"

    Don't get the windows chime when a USB device disconnects even after calling the STOP and DEINIT commands. The chime only happens when I press reset to get out of whatever state the H/W is in i.e. completely unresponsive

    Super User
    February 27, 2021

    What is

    > 1.5K pulldown up on D+

    so is it a pull*down* or a pull*up* (i.e. where is the other end connected)?

    There is no such resistor to be on DM/DP in the 'F4xx. Read the Full-speed OTG PHY subchapter in RM0090.

    JW

    PMath.4Author
    Visitor II
    February 27, 2021

    Operating as device only not OTG. Pullup is standard to indicate to USB host that a device is connected and should be enumerated as full speed.

    There is nothing wrong with the basic USB connection - it works perfectly. The issue is that it isn't releasing and as, unlike the NXP chips, the ST doesn't have a programmable pullup in the UP it has to be external.

    Resetting the processor causes the PC to drop the connection and re-connect so there is something not happening in either STOP or DEINIT that isn't signalling the loss of connection to the PC as it should

    Super User
    February 27, 2021

    > unlike the NXP chips, the ST doesn't have a programmable pullup in the UP it has to be external.

    This for 'F4 is not true. Have you read the chapter I told you to? Have you already thrown out that resistor?

    JW

    PMath.4Author
    Visitor II
    February 27, 2021

    "This for 'F4 is not true. "

    Accepted, but it says that is dependent on using VBUS which isn't configured or connected (optional in CubeMX) and can't be as the pin is in use.

    All irrelevant though as the issue is that a simple reset frees the bus whereas stopping and de-initing doesn't so there is something missing in the implementation of either stop or de-init or I'm missing a step which I can't find

    Super User
    February 27, 2021

    And have you already undone that resistor? It's a 10 seconds operation after the soldering iron has heated up.

    JW

    PMath.4Author
    Visitor II
    February 27, 2021

    Doesn't enumerate at all without the resistor - this discussion is pointless since you are not helping with the actual issue which is the failure of the routines to disconnect - not connect.

    A fixed pullup is there, it is going to stay there, and if sleep won't work then so be it.