GLCD only half screen is working
I am working on Graphic Display(JDH12864E) using STM32L031K6. I have written code and I found that my lcd is printing only half of screen.
For example:- I try to print ("12345678912345") then it prints only ("123456789") it means it is printing only 10 char.
I think the problem is with GLCD_EnableController and GLCD_DisableController function. I tried to search on google i i found that CS1 and CS2 pin is responsible for Left half of screen and Right half of screen but i could not resolve it. please help me to solve this error, so i can print full screen .
my code is :-
/********************************main.c**************************************************/ int main(void) { HAL_Init(); SystemClock_Config(); MX_GPIO_Init(); HAL_Delay(100); GLCD_Initialize(); HAL_Delay(100); GLCD_ClearScreen(); while (1) { GLCD_GoTo(0,0); GLCD_WriteString("Hello World!"); HAL_Delay(10); } } static void MX_GPIO_Init(void) { GPIO_InitTypeDef GPIO_InitStruct = {0}; /* GPIO Ports Clock Enable */ __HAL_RCC_GPIOA_CLK_ENABLE(); __HAL_RCC_GPIOB_CLK_ENABLE(); /*Configure GPIO pin Output Level */ HAL_GPIO_WritePin(GPIOA, GPIO_PIN_0|GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3 |GPIO_PIN_4|GPIO_PIN_5|GPIO_PIN_6|GPIO_PIN_7 |GPIO_PIN_8|GPIO_PIN_9|GPIO_PIN_10|GPIO_PIN_11 |GPIO_PIN_12|GPIO_PIN_13, GPIO_PIN_RESET); /*Configure GPIO pin Output Level */ HAL_GPIO_WritePin(GPIOB, GPIO_PIN_0|GPIO_PIN_1, GPIO_PIN_RESET); /*Configure GPIO pins : PA0 PA1 PA2 PA3 PA4 PA5 PA6 PA7 PA8 PA9 PA10 PA11 PA12 PA13 */ GPIO_InitStruct.Pin = GPIO_PIN_0|GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3 |GPIO_PIN_4|GPIO_PIN_5|GPIO_PIN_6|GPIO_PIN_7 |GPIO_PIN_8|GPIO_PIN_9|GPIO_PIN_10|GPIO_PIN_11 |GPIO_PIN_12|GPIO_PIN_13; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); /*Configure GPIO pins : PB0 PB1 */ GPIO_InitStruct.Pin = GPIO_PIN_0|GPIO_PIN_1; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; HAL_GPIO_Init(GPIOB, &GPIO_InitStruct); } void SystemClock_Config(void) { RCC_OscInitTypeDef RCC_OscInitStruct = {0}; RCC_ClkInitTypeDef RCC_ClkInitStruct = {0}; __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1); RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_MSI; RCC_OscInitStruct.MSIState = RCC_MSI_ON; RCC_OscInitStruct.MSICalibrationValue = 0; RCC_OscInitStruct.MSIClockRange = RCC_MSIRANGE_5; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE; if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) { Error_Handler(); } RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2; RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_MSI; RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1; RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1; if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK) { Error_Handler(); } } /***********************************LCD.c****************************************************/ #include "stm32l0xx_hal.h" #include "graphic_display.h" //#include "lcd.h" #include "font5x8.h" #include "stm32l0xx_hal_gpio.h" // Include the GPIO header unsigned char screen_x = 0; unsigned char screen_y = 0; unsigned char color = 1; void GLCD_Initialize(void) { unsigned char i; GLCD_InitializePorts(); for(i = 0; i < 3; i++) GLCD_WriteCommand((DISPLAY_ON_CMD | ON), i); } void GLCD_Delay_us(uint32_t us) { uint32_t start = SysTick->VAL; uint32_t ticks = (SystemCoreClock / 1000000) * us; while ((start - SysTick->VAL) < ticks); } void GLCD_EnableController(unsigned char controller) { switch(controller){ case 0 : HAL_GPIO_WritePin(KS0108_PORT, KS0108_CS1, GPIO_PIN_RESET); break; case 1 : HAL_GPIO_WritePin(KS0108_PORT, KS0108_CS2, GPIO_PIN_RESET); break; } } void GLCD_DisableController(unsigned char controller) { switch(controller){ case 0 : HAL_GPIO_WritePin(KS0108_PORT, KS0108_CS1, GPIO_PIN_SET); break; case 1 : HAL_GPIO_WritePin(KS0108_PORT, KS0108_CS2, GPIO_PIN_SET); break; } } unsigned char GLCD_ReadStatus(unsigned char controller) { unsigned char status; GPIO_InitTypeDef GPIO_InitStructure; GPIO_InitStructure.Pin = (0xFF << KS0108_D0); GPIO_InitStructure.Mode = GPIO_MODE_INPUT; GPIO_InitStructure.Pull = GPIO_PULLUP; HAL_GPIO_Init(KS0108_PORT, &GPIO_InitStructure); HAL_GPIO_WritePin(KS0108_PORT, KS0108_RS, GPIO_PIN_RESET); GLCD_EnableController(controller); GLCD_Delay_us(3); HAL_GPIO_WritePin(KS0108_PORT, KS0108_EN, GPIO_PIN_SET); GLCD_Delay_us(3); status = ((HAL_GPIO_ReadPin(KS0108_PORT, GPIO_InitStructure.Pin) >> KS0108_D0) & 0xFF); HAL_GPIO_WritePin(KS0108_PORT, KS0108_EN, GPIO_PIN_RESET); GLCD_Delay_us(3); GLCD_DisableController(controller); return status; } void GLCD_WriteCommand(unsigned char commandToWrite, unsigned char controller) { //while (GLCD_ReadStatus(controller) & DISPLAY_STATUS_BUSY); GPIO_InitTypeDef GPIO_InitStructure; GPIO_InitStructure.Pin = (0xFF << KS0108_D0); GPIO_InitStructure.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStructure.Speed = GPIO_SPEED_FREQ_LOW; HAL_GPIO_Init(KS0108_PORT, &GPIO_InitStructure); HAL_GPIO_WritePin(KS0108_PORT, KS0108_RS, GPIO_PIN_RESET); GLCD_EnableController(controller); HAL_GPIO_WritePin(KS0108_PORT, GPIO_InitStructure.Pin, (commandToWrite << KS0108_D0)); commandToWrite ^= 0xFF; HAL_GPIO_WritePin(KS0108_PORT, GPIO_InitStructure.Pin, (commandToWrite << KS0108_D0)); GLCD_Delay_us(3); HAL_GPIO_WritePin(KS0108_PORT, (commandToWrite << KS0108_D0), GPIO_PIN_RESET); HAL_GPIO_WritePin(KS0108_PORT, KS0108_EN, GPIO_PIN_SET); GLCD_Delay_us(3); HAL_GPIO_WritePin(KS0108_PORT, KS0108_EN, GPIO_PIN_RESET); GLCD_DisableController(controller); GLCD_Delay_us(3); } void GLCD_WriteData(unsigned char dataToWrite) { GPIO_InitTypeDef GPIO_InitStructure; GPIO_InitStructure.Pin = (0xFF << KS0108_D0); GPIO_InitStructure.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStructure.Speed = GPIO_SPEED_FREQ_LOW; HAL_GPIO_Init(KS0108_PORT, &GPIO_InitStructure); HAL_GPIO_WritePin(KS0108_PORT, KS0108_RS, GPIO_PIN_SET); HAL_GPIO_WritePin(KS0108_PORT, GPIO_InitStructure.Pin, (dataToWrite << KS0108_D0)); dataToWrite ^= 0xFF; HAL_GPIO_WritePin(KS0108_PORT, GPIO_InitStructure.Pin, (dataToWrite << KS0108_D0)); GLCD_Delay_us(2); HAL_GPIO_WritePin(KS0108_PORT, (dataToWrite << KS0108_D0), GPIO_PIN_RESET); //removing withe box GLCD_EnableController(screen_x / 64); HAL_GPIO_WritePin(KS0108_PORT, KS0108_EN, GPIO_PIN_SET); GLCD_Delay_us(2); HAL_GPIO_WritePin(KS0108_PORT, KS0108_EN, GPIO_PIN_RESET); GLCD_Delay_us(2); GLCD_DisableController(screen_x / 64); // screen_x++; } void GLCD_InitializePorts(void) { // Enable GPIO port clock RCC->IOPENR |= RCC_IOPENR_GPIOAEN; // Enable GPIOA clock // Configure GPIO pins GPIOA->MODER &= ~(GPIO_MODER_MODE0_Msk | GPIO_MODER_MODE1_Msk | GPIO_MODER_MODE2_Msk | GPIO_MODER_MODE3_Msk | GPIO_MODER_MODE4_Msk | GPIO_MODER_MODE5_Msk | GPIO_MODER_MODE6_Msk | GPIO_MODER_MODE7_Msk); GPIOA->MODER |= (GPIO_MODE_OUTPUT_PP << GPIO_MODER_MODE0_Pos) | (GPIO_MODE_OUTPUT_PP << GPIO_MODER_MODE1_Pos) | (GPIO_MODE_OUTPUT_PP << GPIO_MODER_MODE2_Pos) | (GPIO_MODE_OUTPUT_PP << GPIO_MODER_MODE3_Pos) | (GPIO_MODE_OUTPUT_PP << GPIO_MODER_MODE4_Pos) | (GPIO_MODE_OUTPUT_PP << GPIO_MODER_MODE5_Pos) | (GPIO_MODE_OUTPUT_PP << GPIO_MODER_MODE6_Pos) | (GPIO_MODE_OUTPUT_PP << GPIO_MODER_MODE7_Pos); GPIOA->OSPEEDR &= ~(GPIO_OSPEEDER_OSPEED0_Msk | GPIO_OSPEEDER_OSPEED1_Msk | GPIO_OSPEEDER_OSPEED2_Msk | GPIO_OSPEEDER_OSPEED3_Msk | GPIO_OSPEEDER_OSPEED4_Msk | GPIO_OSPEEDER_OSPEED5_Msk | GPIO_OSPEEDER_OSPEED6_Msk | GPIO_OSPEEDER_OSPEED7_Msk); GPIOA->OSPEEDR |= (GPIO_SPEED_FREQ_LOW << GPIO_OSPEEDER_OSPEED0_Pos) | (GPIO_SPEED_FREQ_LOW << GPIO_OSPEEDER_OSPEED1_Pos) | (GPIO_SPEED_FREQ_LOW << GPIO_OSPEEDER_OSPEED2_Pos) | (GPIO_SPEED_FREQ_LOW << GPIO_OSPEEDER_OSPEED3_Pos) | (GPIO_SPEED_FREQ_LOW << GPIO_OSPEEDER_OSPEED4_Pos) | (GPIO_SPEED_FREQ_LOW << GPIO_OSPEEDER_OSPEED5_Pos) | (GPIO_SPEED_FREQ_LOW << GPIO_OSPEEDER_OSPEED6_Pos) | (GPIO_SPEED_FREQ_LOW << GPIO_OSPEEDER_OSPEED7_Pos); // Set GPIO pins to default values GPIOA->ODR = KS0108_CS1 | KS0108_CS2 | KS0108_RS | (0xFF << KS0108_D0); } unsigned char GLCD_ReadByteFromROMMemory(char * ptr) { return *(ptr); } void GLCD_GoTo(unsigned char x, unsigned char y) { unsigned char i; screen_x = x; screen_y = y; for(i = 0; i < (KS0108_SCREEN_WIDTH / 32); i++)//64 { GLCD_WriteCommand((DISPLAY_SET_Y | 0), i); GLCD_WriteCommand((DISPLAY_SET_X | y), i); GLCD_WriteCommand((DISPLAY_START_LINE | 0), i); } GLCD_WriteCommand((DISPLAY_SET_Y | (x % 64)), (x / 64)); GLCD_WriteCommand((DISPLAY_SET_X | y), (x / 64)); } void GLCD_ClearScreen(void) { unsigned char i, j; for(j = 0; j < KS0108_SCREEN_HEIGHT / 8; j++) { GLCD_GoTo(0, j); for(i = 0; i < KS0108_SCREEN_WIDTH; i++) GLCD_WriteData(0x00); } } void GLCD_WriteChar(char charToWrite) { char i; charToWrite -= ' '; for(i = 0; i < 5; i++) GLCD_WriteData(GLCD_ReadByteFromROMMemory((char *)(font5x8 + (5 * charToWrite) + i))); GLCD_WriteData(0x00); } void GLCD_WriteString(char * stringToWrite) { while(*stringToWrite) GLCD_WriteChar(*stringToWrite++); } void delay_us(uint32_t us) { uint32_t start = SysTick->VAL; uint32_t ticks = (SystemCoreClock / 1000000) * us; while ((start - SysTick->VAL) < ticks); } /***********************************LCD.c**************************************************************/ #define KS0108_SCREEN_WIDTH 128 #define KS0108_SCREEN_HEIGHT 64 #define DISPLAY_SET_Y 0x40 #define DISPLAY_SET_X 0xB8 #define DISPLAY_START_LINE 0xC0 #define DISPLAY_ON_CMD 0x3E //#define ON 0x01 //#define OFF 0x00 #define DISPLAY_STATUS_BUSY 0x80 #define ON (1) #define OFF (0) #define KS0108_DATA_PORT GPIOA #define KS0108_PORT GPIOA #define KS0108_RS GPIO_PIN_8 #define KS0108_RW GPIO_PIN_13 #define KS0108_EN GPIO_PIN_9 #define KS0108_CS1 GPIO_PIN_11 #define KS0108_CS2 GPIO_PIN_10 //#define KS0108_CS3 GPIO_PIN_13 #define KS0108_D0 0 /******************************************************************************************************/