H723-Ethernet_LWIP Ping problem
Hello ST Community,
I am currently working with the Nucleo H723ZG board and facing issues establishing a ping response using the LWIP stack. Despite following various examples and configurations, I have been unable to get it to respond to pings. Here are the details of my setup:
- Development Environment: STM32CubeIDE V1.17 and STM32CubeMX V6.13.0
- Configuration:
- I have not used RTOS.
- I configured the Ethernet settings according to package examples.
- :C:\....\STM32Cube\Repository\STM32Cube_FW_H7_V1.12.1\Projects\NUCLEO-H723ZG\Applications\LwIP\LwIP_UDP_Echo_Server
- I ensured that the Ethernet cable was connected properly and used a direct connection to my pc.
I have tried multiple versions of the H7 package ( 1.12.1 - 1.12.0 - 1.11.1 - 1.11.0 - 1.10.0 ) and tested various configurations without success. The ping command consistently results in "destination host unreachable."Could anyone provide insights or suggestions on what might be missing or misconfigured?
//*****************************
My Ethernet configuration :

//*****************************
Ethernet GPIO Configuration:

//*****************************
MPU Configuration :

//*****************************
LWIP configuration :




I added this part to the STM32H723ZGTX_FLASH.ld file:
//************************************************************************************
..........
. = ALIGN(8);
} >RAM_D1
.lwip_sec (NOLOAD) : {
. = ABSOLUTE(0x30000000);
*(.RxDecripSection)
. = ABSOLUTE(0x30000080);
*(.TxDecripSection)
. = ABSOLUTE(0x30000100);
*(.Rx_PoolSection)
} >RAM_D2 AT> FLASH
/* Remove information from the standard libraries */
/DISCARD/ :
//**********************************************************
and its result is like this:

My main.c code:
//**********************************************************
/* USER CODE BEGIN PV */
extern struct netif gnetif;
/* USER CODE END PV */
++++++++++++++++++++++++++++++++++++++++++++++++++++
in int main(void)
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
ethernetif_input(&gnetif);
sys_check_timeouts();
}
//**********************************************************
ressult:

My CPU clock is 520Mhz. I am sure the hardware has no problem because I can give a ping from the st package example.
But when I configure according that example it does not work.
.Thank you for your assistance!Best regards,
[Your Name]