H743ZI2 USB OTG with external power source
Hello,
I have a Nucleo H743ZI2 on which I am communicating with the micro AB USB port through USB OTG. Up until now I always had the main USB (STlink) plugged in to power the board. Eventually I want to power the nucleo board with an external 3.3 power source (another board in the system).
However whenever I do that (i.e. power the H7 with the external 3.3V source), the USB OTG won't enumerate and get detected by the PC.
The datasheet is not helping, actually, my understanding is that ST actually recommends the use of the an external power supply when using USB OTG. Quote:
1.It is recommended to power the Nucleo-144 board with an external power supply when using USB OTG or host function.I am using the USB OTG as device only, SOF and VBus all disabled.
Does anyone know what I am missing here?
cheers