HAL and MISRA C compliance problem
I've started a project with HAL library using stm32cubemx. I'm using keil for my programming and I've added PC-Lint (MISRAC checker) to check C standards. But when I run PC-lint to check MISRA C rules, I will receive lots of MISRA C 2012 violation rules that arises from HAL commands. Note, I have not entered any other codes but those which generated by stm32cube.
For example the generated files contains these two lines:
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
__attribute__((section(".revsh_text"))) __STATIC_INLINE __ASM int16_t __REVSH(int16_t value)but I receive these errors consequently:
: Note 934: Taking address of near auto variable 'GPIO_InitStruct' (arg. no. 2) [MISRA 2012 Rule 1.3, required]
__attribute__((section(".revsh_text"))) __STATIC_INLINE __ASM int16_t __REVSH(int16_t value)I also receive lots of more errors either. According to this , HAL is in compliance with MISRA C 2012. What is wrong?