[HAL Bug Report] STM32G474 Cannot use "HAL_ADC_Start_DMA" with ADC5 when ADC3 and ADC4 configured in dual regular mode
Here is the code in question:
HAL_StatusTypeDef HAL_ADC_Start_DMA(ADC_HandleTypeDef *hadc, uint32_t *pData, uint32_t Length)
{
HAL_StatusTypeDef tmp_hal_status;
#if defined(ADC_MULTIMODE_SUPPORT)
uint32_t tmp_multimode_config = LL_ADC_GetMultimode(__LL_ADC_COMMON_INSTANCE(hadc->Instance));
#endif
/* Check the parameters */
assert_param(IS_ADC_ALL_INSTANCE(hadc->Instance));
/* Perform ADC enable and conversion start if no conversion is on going */
if (LL_ADC_REG_IsConversionOngoing(hadc->Instance) == 0UL)
{
/* Process locked */
__HAL_LOCK(hadc);
#if defined(ADC_MULTIMODE_SUPPORT)
/* Ensure that multimode regular conversions are not enabled. */
/* Otherwise, dedicated API HAL_ADCEx_MultiModeStart_DMA() must be used. */
if ((tmp_multimode_config == LL_ADC_MULTI_INDEPENDENT)
|| (tmp_multimode_config == LL_ADC_MULTI_DUAL_INJ_SIMULT)
|| (tmp_multimode_config == LL_ADC_MULTI_DUAL_INJ_ALTERN)
)
#endifSince ADC5 shares its multimode configuration register with ADC3 and ADC4, trying to invoke HAL_ADC_Start_DMA with hadc5 when ADC3 and ADC4 are configured for dual regular mode returns HAL error.
I tried modifying the code as shown below and ADC5 works without issues (samples are accurate, DMA callbacks invoked at expected rate).
HAL_StatusTypeDef User_ADC_Start_DMA(ADC_HandleTypeDef *hadc, uint32_t *pData, uint32_t Length)
{
HAL_StatusTypeDef tmp_hal_status;
#if defined(ADC_MULTIMODE_SUPPORT)
uint32_t tmp_multimode_config = LL_ADC_GetMultimode(__LL_ADC_COMMON_INSTANCE(hadc->Instance));
#endif
/* Check the parameters */
assert_param(IS_ADC_ALL_INSTANCE(hadc->Instance));
/* Perform ADC enable and conversion start if no conversion is on going */
if (LL_ADC_REG_IsConversionOngoing(hadc->Instance) == 0UL)
{
/* Process locked */
__HAL_LOCK(hadc);
#if defined(ADC_MULTIMODE_SUPPORT)
/* Ensure that multimode regular conversions are not enabled. */
/* Otherwise, dedicated API HAL_ADCEx_MultiModeStart_DMA() must be used. */
if ((ADC_IS_INDEPENDENT(hadc))
|| (tmp_multimode_config == LL_ADC_MULTI_INDEPENDENT)
|| (tmp_multimode_config == LL_ADC_MULTI_DUAL_INJ_SIMULT)
|| (tmp_multimode_config == LL_ADC_MULTI_DUAL_INJ_ALTERN)
)
#endifI was wondering if this is going to be addressed in a HAL update?
Thank you.