HAL_Delay hangs after jumping from bootloader to FreeRTOS app (using TIM14 as tick source)
Hello,
I am working on an STM32F446RE with a custom bootloader and FreeRTOS application.
Bootloader address: 0x08000000
Application address: 0x0800C000
The bootloader successfully jumps to the application by setting MSP, PC, and SCB->VTOR.
In my application, I configured FreeRTOS to use a hardware timer (TIM14) instead of SysTick as the OS tick source.
Problem:
When I flash the application directly, it runs fine.
But when I run through the bootloader, the application stops working as soon as it calls HAL_Delay(). If I comment out HAL_Delay(), the app continues normally. After the RTOS kernel starts, I get a HardFault on the first interrupt.
I suspect this is related to SysTick still being dirty from the bootloader, while my application is configured to use TIMx as the tick source.
My questions:
What is the recommended way to cleanly reinitialize the HAL tick and interrupt system after jumping from a bootloader to an application that uses TIMx instead of SysTick?
Should I override HAL_InitTick/HAL_GetTick in the application so that HAL_Delay() works with FreeRTOS (using TIMx ticks)?
If HAL_Delay() must work before FreeRTOS scheduler starts, should I explicitly reconfigure SysTick in the application even though FreeRTOS uses TIM14?
Is there a recommended sequence of peripheral deinitialization in the bootloader to avoid SysTick/interrupt leftovers?
Extra info:
Toolchain: GCC (CubeIDE, no optimizations)
Bootloader disables SysTick (SysTick->CTRL=0; SysTick->LOAD=0; SysTick->VAL=0;) before jump.
Application runs fine standalone, fails only after bootloader jump when HAL_Delay() is called.
Thanks in advance for guidance.