HAL_DMA_RegisterCallback with SPI
Hi,
I'm just struggling with the same problem. I use SPI with DMA non-circular mode and want a callback for receive complete.
I can set the callback function with HAL_DMA_RegisterCallback but in HAL_SPI_TransmitReceive_DMA it will be overwritten:
/* Set the SPI Tx/Rx DMA Half transfer complete callback */
hspi->hdmarx->XferHalfCpltCallback = SPI_DMAHalfTransmitReceiveCplt;
hspi->hdmarx->XferCpltCallback = SPI_DMATransmitReceiveCplt;
Edit: Post moved from original thread How to know the when the DMA transfer done?, to give a chance to be answered. Please precise if you are using U5 as original one.