Skip to main content
Visitor II
January 14, 2023
Solved

HAL documentation has some serious error related to HAL_GetTick

  • January 14, 2023
  • 2 replies
  • 1360 views

The HAL L4 page 38 - but I saw it more also in other doc - has an error how to use HAL_GetTick for timeout:

HAL_StatusTypeDef HAL_PPP_Process(PPP_HandleTypeDef)

timeout = HAL_GetTick() + LOCAL_PROCESS_TIMEOUT;

while(ProcessOngoing)

if (HAL_GetTick() ≥ timeout)

Why I think this is wrong: HAL_GetTick returns a uint32_t counter (at least in the ST libs I checked). This unsigned 32 bit value default increments 1000 times/s and overruns from 0xFFFFFFFF to 0x00000000 after ~49.71 days. Suppose the process started at Tick 0xFFFEDCBA. After adding the the wanted timeout (ex. ~74s), the timeout must trigger when Tick reaches 0x00000123. That value will be correctly calculated in the ST example. But 1 tick after the process started, Tick will be 0xFFFFEDCBB. Since that's bigger than the computed end value 0x123, the code incorrectly triggers a timeout after 1ms instead of 74s.

I believe it's better to do it this way:

uint32_t processStart = HAL_GetTick ();

....

if ((HAL_GetTick () - processStart) >= myAppTimeOut) { } //Timeout.

Here one can see this in the 2's complement result at the moment timeout triggers:

0693W00000Y8FFDQA3.pngThe relative timing code will generate at assembly level an overflow once Tick rolls over to 0x0, but in C that flag is discarded. As long as HAL_GetTick did not roll over to 0x0, the core reports no overflow. The relative timeout will be correctly handled in both cases (regardless if there's an overflow or not).

    This topic has been closed for replies.
    Best answer by Patrice LF

    Hi @EGi​ 

    Thank your for spotting this documentation issue that mismatches with actual STM32Cube HAL drivers timeout implementation. It was reported internally for a fix in forthcoming releases of User Manual of STM32 series HAL and low-layer drivers.

    Regards

    Patrice

    2 replies

    Explorer II
    January 14, 2023

    This is a very old problem that has been reported many times before...

    https://community.st.com/s/question/0D50X00009XkgXi/years-on-continue-to-see-the-same-bad-timeout-code

    Technical Moderator
    February 22, 2023

    Hi @EGi​ 

    Thank your for spotting this documentation issue that mismatches with actual STM32Cube HAL drivers timeout implementation. It was reported internally for a fix in forthcoming releases of User Manual of STM32 series HAL and low-layer drivers.

    Regards

    Patrice