HAL_I2C_GetState does not work after task creation and before osKernelStart()
Hello
Using FreeRTOS on F412.
Considering this simple function:
void initFromEEprom(void) {
uint8_t data[10];
HAL_StatusTypeDef err = HAL_I2C_Mem_Read_DMA(&hi2c1,
160, 8,
16,
(uint8_t*)data,
7);
assert(err == HAL_OK);
while (HAL_I2C_GetState(&hi2c1) != HAL_I2C_STATE_READY) {
}
}
It works when called within a running task.
It works when called before osKernelStart() AND before creation of any task.
Now, if I do something like this:
int main(void)
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_DMA_Init();
MX_I2C1_Init();
osThreadDef(defaultTask, StartDefaultTask, osPriorityNormal, 0, 128);
defaultTaskHandle = osThreadCreate(osThread(defaultTask), NULL);
initFromEEprom();
osKernelStart();
while (1) {
}
}In this case the HAL_I2C_GetState() always returns HAL_I2C_STATE_BUSY_RX.
btw, It took me some hours to understand that this was the reason of my big project failure...
Now, I can do a workaround but looking as osThreadCreate code, I was not able to figure out why this behaviour.
Can anybody explain?
Thanks
Julien