Question
HAL_NVIC_EnableIRQ does not end
// DMA RX 설정
__HAL_RCC_DMA1_CLK_ENABLE(); // DMA1 클럭 활성화
hdma_rx.Instance = DMA_USART1;
hdma_rx.Init.Request = DMA_REQUEST_USART1_RX;
hdma_rx.Init.Direction = DMA_PERIPH_TO_MEMORY;
hdma_rx.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_rx.Init.MemInc = DMA_MINC_ENABLE;
hdma_rx.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE;
hdma_rx.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE;
hdma_rx.Init.Mode = DMA_CIRCULAR; // 순환 모드
hdma_rx.Init.Priority = DMA_PRIORITY_LOW;
if (HAL_DMA_Init(&hdma_rx) != HAL_OK) { return IMU_INIT_FAILED; }
__HAL_LINKDMA(&huart, hdmarx, hdma_rx);
if (HAL_UART_Receive_DMA(&huart, &q_buf[0], DMA_BUFFER_IMU) != HAL_OK) { return IMU_INIT_FAILED; }
Delay_ms(1);
__HAL_UART_CLEAR_FLAG(&huart, UART_FLAG_IDLE);
HAL_NVIC_SetPriority(UART_IMU_IRQ, IT_PRIOR_IMU_PREM, IT_PRIOR_IMU_SUB); // Set priority
HAL_NVIC_EnableIRQ(UART_IMU_IRQ); // Enable IRQ
__HAL_UART_ENABLE_IT(&huart, UART_IT_IDLE);
__HAL_UART_CLEAR_FLAG(&huart, UART_FLAG_IDLE);
return IMU_INIT_SUCCESS;
}
literally, HAL_NVIC_EnableIRQ does not end...
the parameters in code is as follows:
DMA_BUFFER_IMU : 128
UART_IMU_IRQ : USART1_IRQn
IT_PRIOR_IMU_PREM : 1
IT_PRIOR_IMU_SUB : 1