Skip to main content
Graduate II
January 23, 2025
Solved

HAL_UART_Receive_IT is not working

  • January 23, 2025
  • 6 replies
  • 4700 views

Originally a reply in this thread - split as a separate question.


Hello 

My blocking mode is working with "HAL_UART_Receive(&huart4, temp, 1, 100);"

Nonblocking mode is not working

Can you suggest anything to check?

I have defined as said

 

/* USER CODE BEGIN 2 */

HAL_UART_Receive_IT(&huart4, temp, 1);

/* USER CODE END 2 */

 

and

 

/* USER CODE BEGIN 4 */

void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
{
 HAL_UART_Receive_IT(&huart4, temp, 1);
 HAL_UART_Transmit(&huart4, temp, 1, 100);
}

/* USER CODE END 4 */

 

    This topic has been closed for replies.
    Best answer by KaushikSTM32

     

    Yes sir its enabled.

    Port pins are also correct.

    void HAL_UART_MspInit(UART_HandleTypeDef* huart)
    {
     GPIO_InitTypeDef GPIO_InitStruct = {0};
     RCC_PeriphCLKInitTypeDef PeriphClkInit = {0};
     if(huart->Instance==USART3)
     {
     /* USER CODE BEGIN USART3_MspInit 0 */
    
     /* USER CODE END USART3_MspInit 0 */
    
     /** Initializes the peripherals clocks
     */
     PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_USART3;
     PeriphClkInit.Usart3ClockSelection = RCC_USART3CLKSOURCE_PCLK1;
     if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
     {
     Error_Handler();
     }
    
     /* Peripheral clock enable */
     __HAL_RCC_USART3_CLK_ENABLE();
    
     __HAL_RCC_GPIOC_CLK_ENABLE();
     /**USART3 GPIO Configuration
     PC10 ------> USART3_TX
     PC11 ------> USART3_RX
     */
     GPIO_InitStruct.Pin = GPIO_PIN_10|GPIO_PIN_11;
     GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
     GPIO_InitStruct.Pull = GPIO_NOPULL;
     GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
     GPIO_InitStruct.Alternate = GPIO_AF7_USART3;
     HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
    
     /* USART3 interrupt Init */
     HAL_NVIC_SetPriority(USART3_IRQn, 0, 0);
     HAL_NVIC_EnableIRQ(USART3_IRQn);
     /* USER CODE BEGIN USART3_MspInit 1 */
    
     /* USER CODE END USART3_MspInit 1 */
    
     }

      

    6 replies

    Technical Moderator
    January 23, 2025

    Hello @KaushikSTM32 

    Did you enable the UART global interrupt please?

    Super User
    January 23, 2025

    @KaushikSTM32 wrote:

    Nonblocking mode is not working


    Define "not working"

    • Does not build?
    • Crashes?
    • Receives junk?
    • other??

    Have you enabled the interrupts?

    Graduate II
    January 23, 2025

    Hello Andew and Saket

    Well I have used putty, In blocking it was receiving what has been sent and also my toggle pin is working in while loop.

    In non blocking, toggle pin stopped and also didn't received any data from controller.

    What shall I do next?

    Technical Moderator
    January 23, 2025

    Hello @KaushikSTM32 

    Could you please share your entire code? This will allow us to assist you more effectively.

    Graduate II
    January 23, 2025

    Replied below

    Graduate II
    January 24, 2025

    sir,

    Implemented and rechecked in blocking mode, Its working fine.

    But facing the same problem with non blocking interrupt mode: when I entered a thing on serial terminal(putty) it got hanged and stopped my toggling also. code is attached.

     

    /* USER CODE BEGIN Header */
    
    /**
    
    ******************************************************************************
    
    * @file : main.c
    
    * @brief : Main program body
    
    ******************************************************************************
    
    * @attention
    
    *
    
    * Copyright (c) 2025 STMicroelectronics.
    
    * All rights reserved.
    
    *
    
    * This software is licensed under terms that can be found in the LICENSE file
    
    * in the root directory of this software component.
    
    * If no LICENSE file comes with this software, it is provided AS-IS.
    
    *
    
    ******************************************************************************
    
    */
    
    /* USER CODE END Header */
    
    /* Includes ------------------------------------------------------------------*/
    
    #include "main.h"
    
     
    
    /* Private includes ----------------------------------------------------------*/
    
    /* USER CODE BEGIN Includes */
    
     
    
    /* USER CODE END Includes */
    
     
    
    /* Private typedef -----------------------------------------------------------*/
    
    /* USER CODE BEGIN PTD */
    
     
    
    /* USER CODE END PTD */
    
     
    
    /* Private define ------------------------------------------------------------*/
    
    /* USER CODE BEGIN PD */
    
    uint8_t UART4_rxBuffer[12] = {0};
    
    /* USER CODE END PD */
    
     
    
    /* Private macro -------------------------------------------------------------*/
    
    /* USER CODE BEGIN PM */
    
     
    
    /* USER CODE END PM */
    
     
    
    /* Private variables ---------------------------------------------------------*/
    
    UART_HandleTypeDef huart4;
    
    unsigned char RXcplt;
    
    /* USER CODE BEGIN PV */
    
     
    
    /* USER CODE END PV */
    
     
    
    /* Private function prototypes -----------------------------------------------*/
    
    void SystemClock_Config(void);
    
    static void MX_GPIO_Init(void);
    
    static void MX_UART4_Init(void);
    
    /* USER CODE BEGIN PFP */
    
     
    
    /* USER CODE END PFP */
    
     
    
    /* Private user code ---------------------------------------------------------*/
    
    /* USER CODE BEGIN 0 */
    
     
    
    /* USER CODE END 0 */
    
     
    
    /**
    
    * @brief The application entry point.
    
    * @retval int
    
    */
    
    int main(void)
    
    {
    
     
    
    /* USER CODE BEGIN 1 */
    
     
    
    /* USER CODE END 1 */
    
     
    
    /* MCU Configuration--------------------------------------------------------*/
    
     
    
    /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
    
    HAL_Init();
    
     
    
    /* USER CODE BEGIN Init */
    
     
    
    /* USER CODE END Init */
    
     
    
    /* Configure the system clock */
    
    SystemClock_Config();
    
     
    
    /* USER CODE BEGIN SysInit */
    
     
    
    /* USER CODE END SysInit */
    
     
    
    /* Initialize all configured peripherals */
    
    MX_GPIO_Init();
    
    MX_UART4_Init();
    
    /* USER CODE BEGIN 2 */
    
    HAL_UART_Receive_IT (&huart4, UART4_rxBuffer, 5);
    
    RXcplt = 0;
    
    /* USER CODE END 2 */
    
     
    
    /* Infinite loop */
    
    /* USER CODE BEGIN WHILE */
    
    while (1)
    
    {
    
    /* USER CODE END WHILE */
    
    // HAL_UART_Receive(&huart4, UART4_rxBuffer, 5, 1000);
    
    // HAL_UART_Transmit(&huart4, UART4_rxBuffer, 5, 1000);
    
    if(RXcplt)
    
    {
    
    RXcplt = 0;
    
    HAL_UART_Transmit(&huart4, UART4_rxBuffer, 5, 1000);
    
    HAL_UART_Receive_IT(&huart4, UART4_rxBuffer, 5);
    
    }
    
    HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_4);
    
    HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_5);
    
    /* USER CODE BEGIN 3 */
    
    }
    
    /* USER CODE END 3 */
    
    }
    
     
    
    /**
    
    * @brief System Clock Configuration
    
    * @retval None
    
    */
    
    void SystemClock_Config(void)
    
    {
    
    RCC_OscInitTypeDef RCC_OscInitStruct = {0};
    
    RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
    
     
    
    /** Configure the main internal regulator output voltage
    
    */
    
    HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1);
    
     
    
    /** Initializes the RCC Oscillators according to the specified parameters
    
    * in the RCC_OscInitTypeDef structure.
    
    */
    
    RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
    
    RCC_OscInitStruct.HSIState = RCC_HSI_ON;
    
    RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
    
    RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
    
    RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
    
    RCC_OscInitStruct.PLL.PLLM = RCC_PLLM_DIV4;
    
    RCC_OscInitStruct.PLL.PLLN = 75;
    
    RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
    
    RCC_OscInitStruct.PLL.PLLQ = RCC_PLLQ_DIV2;
    
    RCC_OscInitStruct.PLL.PLLR = RCC_PLLR_DIV2;
    
    if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
    
    {
    
    Error_Handler();
    
    }
    
     
    
    /** Initializes the CPU, AHB and APB buses clocks
    
    */
    
    RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
    
    |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
    
    RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
    
    RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
    
    RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
    
    RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
    
     
    
    if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_4) != HAL_OK)
    
    {
    
    Error_Handler();
    
    }
    
    }
    
     
    
    /**
    
    * @brief UART4 Initialization Function
    
    * @PAram None
    
    * @retval None
    
    */
    
    static void MX_UART4_Init(void)
    
    {
    
     
    
    /* USER CODE BEGIN UART4_Init 0 */
    
     
    
    /* USER CODE END UART4_Init 0 */
    
     
    
    /* USER CODE BEGIN UART4_Init 1 */
    
     
    
    /* USER CODE END UART4_Init 1 */
    
    huart4.Instance = UART4;
    
    huart4.Init.BaudRate = 115200;
    
    huart4.Init.WordLength = UART_WORDLENGTH_8B;
    
    huart4.Init.StopBits = UART_STOPBITS_1;
    
    huart4.Init.Parity = UART_PARITY_NONE;
    
    huart4.Init.Mode = UART_MODE_TX_RX;
    
    huart4.Init.HwFlowCtl = UART_HWCONTROL_NONE;
    
    huart4.Init.OverSampling = UART_OVERSAMPLING_16;
    
    huart4.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
    
    huart4.Init.ClockPrescaler = UART_PRESCALER_DIV1;
    
    huart4.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
    
    if (HAL_UART_Init(&huart4) != HAL_OK)
    
    {
    
    Error_Handler();
    
    }
    
    if (HAL_UARTEx_SetTxFifoThreshold(&huart4, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK)
    
    {
    
    Error_Handler();
    
    }
    
    if (HAL_UARTEx_SetRxFifoThreshold(&huart4, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK)
    
    {
    
    Error_Handler();
    
    }
    
    if (HAL_UARTEx_DisableFifoMode(&huart4) != HAL_OK)
    
    {
    
    Error_Handler();
    
    }
    
    /* USER CODE BEGIN UART4_Init 2 */
    
     
    
    /* USER CODE END UART4_Init 2 */
    
     
    
    }
    
     
    
    /**
    
    * @brief GPIO Initialization Function
    
    * @PAram None
    
    * @retval None
    
    */
    
    static void MX_GPIO_Init(void)
    
    {
    
    GPIO_InitTypeDef GPIO_InitStruct = {0};
    
    /* USER CODE BEGIN MX_GPIO_Init_1 */
    
    /* USER CODE END MX_GPIO_Init_1 */
    
     
    
    /* GPIO Ports Clock Enable */
    
    __HAL_RCC_GPIOA_CLK_ENABLE();
    
    __HAL_RCC_GPIOC_CLK_ENABLE();
    
     
    
    /*Configure GPIO pin Output Level */
    
    HAL_GPIO_WritePin(GPIOA, GPIO_PIN_4|GPIO_PIN_5, GPIO_PIN_RESET);
    
     
    
    /*Configure GPIO pins : PA4 PA5 */
    
    GPIO_InitStruct.Pin = GPIO_PIN_4|GPIO_PIN_5;
    
    GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
    
    GPIO_InitStruct.Pull = GPIO_NOPULL;
    
    GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
    
    HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
    
     
    
    /* USER CODE BEGIN MX_GPIO_Init_2 */
    
    /* USER CODE END MX_GPIO_Init_2 */
    
    }
    
     
    
    /* USER CODE BEGIN 4 */
    
    void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
    
    {
    
    RXcplt = 1;
    
    }
    
    /* USER CODE END 4 */
    
     
    
    /**
    
    * @brief This function is executed in case of error occurrence.
    
    * @retval None
    
    */
    
    void Error_Handler(void)
    
    {
    
    /* USER CODE BEGIN Error_Handler_Debug */
    
    /* User can add his own implementation to report the HAL error return state */
    
    __disable_irq();
    
    while (1)
    
    {
    
    }
    
    /* USER CODE END Error_Handler_Debug */
    
    }
    
     
    
    #ifdef USE_FULL_ASSERT
    
    /**
    
    * @brief Reports the name of the source file and the source line number
    
    * where the assert_param error has occurred.
    
    * @PAram file: pointer to the source file name
    
    * @PAram line: assert_param error line source number
    
    * @retval None
    
    */
    
    void assert_failed(uint8_t *file, uint32_t line)
    
    {
    
    /* USER CODE BEGIN 6 */
    
    /* User can add his own implementation to report the file name and line number,
    
    ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
    
    /* USER CODE END 6 */
    
    }
    
    #endif /* USE_FULL_ASSERT */
     
    Graduate II
    January 24, 2025

    Attach your IOC file

    Graduate II
    January 24, 2025

    Yes sir, file is attached.

    Graduate II
    January 25, 2025

    void UART4_IRQHandler(void) this ISR routine is not executed while receiving.

    Graduate II
    January 25, 2025

    Check the stm32xxxhal_msp.c file to be sure any reference to UART4 are there. May look something like this though port pins might be different. 

    void HAL_UART_MspInit(UART_HandleTypeDef* huart)
    {
     GPIO_InitTypeDef GPIO_InitStruct = {0};
     RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
     if(huart->Instance==UART4)
     {
     /* USER CODE BEGIN UART4_MspInit 0 */
    
     /* USER CODE END UART4_MspInit 0 */
    
     /** Initializes the peripherals clock
     */
     PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_UART4;
     PeriphClkInitStruct.Usart234578ClockSelection = RCC_USART234578CLKSOURCE_D2PCLK1;
     if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
     {
     Error_Handler();
     }
    
     /* Peripheral clock enable */
     __HAL_RCC_UART4_CLK_ENABLE();
    
     __HAL_RCC_GPIOA_CLK_ENABLE();
     /**UART4 GPIO Configuration
     PA0 ------> UART4_TX
     PA1 ------> UART4_RX
     */
     GPIO_InitStruct.Pin = GPIO_PIN_0|GPIO_PIN_1;
     GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
     GPIO_InitStruct.Pull = GPIO_NOPULL;
     GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
     GPIO_InitStruct.Alternate = GPIO_AF8_UART4;
     HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
    
     /* UART4 interrupt Init */
     HAL_NVIC_SetPriority(UART4_IRQn, 0, 0);
     HAL_NVIC_EnableIRQ(UART4_IRQn);
     /* USER CODE BEGIN UART4_MspInit 1 */
    
     /* USER CODE END UART4_MspInit 1 */
     }

     

    KaushikSTM32AuthorAnswer
    Graduate II
    January 25, 2025

     

    Yes sir its enabled.

    Port pins are also correct.

    void HAL_UART_MspInit(UART_HandleTypeDef* huart)
    {
     GPIO_InitTypeDef GPIO_InitStruct = {0};
     RCC_PeriphCLKInitTypeDef PeriphClkInit = {0};
     if(huart->Instance==USART3)
     {
     /* USER CODE BEGIN USART3_MspInit 0 */
    
     /* USER CODE END USART3_MspInit 0 */
    
     /** Initializes the peripherals clocks
     */
     PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_USART3;
     PeriphClkInit.Usart3ClockSelection = RCC_USART3CLKSOURCE_PCLK1;
     if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
     {
     Error_Handler();
     }
    
     /* Peripheral clock enable */
     __HAL_RCC_USART3_CLK_ENABLE();
    
     __HAL_RCC_GPIOC_CLK_ENABLE();
     /**USART3 GPIO Configuration
     PC10 ------> USART3_TX
     PC11 ------> USART3_RX
     */
     GPIO_InitStruct.Pin = GPIO_PIN_10|GPIO_PIN_11;
     GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
     GPIO_InitStruct.Pull = GPIO_NOPULL;
     GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
     GPIO_InitStruct.Alternate = GPIO_AF7_USART3;
     HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
    
     /* USART3 interrupt Init */
     HAL_NVIC_SetPriority(USART3_IRQn, 0, 0);
     HAL_NVIC_EnableIRQ(USART3_IRQn);
     /* USER CODE BEGIN USART3_MspInit 1 */
    
     /* USER CODE END USART3_MspInit 1 */
    
     }