HAL USB_CoreReset times out on the CM4 core of a Nucleo-H745zi-q
Attempting to get USB CDC running on the CM4 core of a stock Nucleo-H745zi-q board. USB_CoreReset() times out waiting for a soft reset. Any help would be greatly appreciated.
Timeout is in stm32h7xx_ll_usb.c, lines 1456-1469:
/* Core Soft Reset */
count = 0U;
USBx->GRSTCTL |= USB_OTG_GRSTCTL_CSRST;
do
{
count++;
if (count > 200000U)
{
return HAL_TIMEOUT;
}
} while ((USBx->GRSTCTL & USB_OTG_GRSTCTL_CSRST) == USB_OTG_GRSTCTL_CSRST);USB clock is RC48
Project built with CubeMX V6.6.1, CubeIDE V1.10.1, Firmware FW_H7 V1.10.0
I moved the USB from the CM4 core to the CM7, and this issue does not occur.