Hard Fault
Hello all ,
I am facing a issue of hard fault because of some reason however after analyzing issue I suspect this could be due to use of structure having uint64_t variable having bit fielding. I have also attached snapshot of issue which I am facing(Precise data access violation).

typedef struct _st_device_info_payload
{
uint64_t IMEI : 50;
uint64_t BLE_MAC_ID : 48;
uint64_t WiFi_MAC_ID : 48;
uint16_t Server_Port;
uint64_t SIM_ICCID_1 :6;
uint64_t SIM_ICCID_2 :64;
char Server_Domain_Name[20];
char APN[20];
}st_device_info_payload;
Please confirm these few points.
1. Can I use uint64_t for STM32H7 MCU.
2. Can we use bit fielding for uint64_t variable for stm32h7.