Hard fault at SystemClock_Config after jumping from OpenBootloader to application
Hello Community,
I am getting a hard fault at SystemClock_Config when executing the application after jumping from OpenBootloader. It is confirmed by single stepping through application. The bootloader uses HSI (16MHz) and PLL to operate at 72MHz and the application uses HSE (24MHz) and PLL to run at 170MHz. When the application clock is configured to use HSI and run at 170MHz it works fine.
So what might be missing here?
Any hints?