Skip to main content
Visitor II
December 8, 2025
Question

HardFault & DMA Descriptor Memory Issues in STM32F746G-Discovery Ethernet (LwIP) – Need Guidance for Cloud POST API Integration

  • December 8, 2025
  • 0 replies
  • 97 views

Post edited by ST moderator to be inline with the community rules for the code sharing. In next time please use </> button to paste your code and a linker script content. Please read this post: How to insert source code.

Hello Community,

I am working on STM32F746G-Discovery and trying to send ADC sensor data to a cloud server using Ethernet.
Cloud API details:

URL: https://iot.hummingbirdtek.com/api/data
Method: POST
Content-Type: application/json

What I Have Done:

  1. Enabled Ethernet (RMII) in CubeMX

  2. Enabled LwIP, set static IP

  3. Enabled ADC1, UART6 for debug

  4. Generated code (AC6/GCC)

  5. Added code to format JSON and send to cloud using http_post

    Issues I am facing:

    1) HardFault occurs after LwIP initialization

    The crash happens during:

    MX_LWIP_Init();
    netif_set_up();


    2) DMA Descriptor Memory Configuration Errors

    Compiler shows errors like:

    DMARxDscrTab memory out of range
    or
    aggregate value used where integer expected

    I suspect incorrect MPU/Alignment/Section placement for:

    ETH_DMADescTypeDef DMARxDscrTab[ETH_RX_DESC_CNT] __attribute__((section(".RxDecripSection")));
    ETH_DMADescTypeDef DMATxDscrTab[ETH_TX_DESC_CNT] __attribute__((section(".TxDecripSection")));


    I am not sure how this should be configured in CubeMX linker settings for STM32F746.

    3) Need guidance for correct .ioc Ethernet/LwIP configuration

    Specifically:

    • ETH clock settings

    • RMII pins required

    • LwIP static IP configuration

    • Required settings in lwipopts.h

    • Whether mbedTLS is required for HTTPS POST

    • If any official ST example project exists for STM32F746 + LwIP + HTTP POST

      4) Request

      Can someone please guide me with:

      ✔ Correct CubeMX IOC configuration steps
      ✔ Correct linker script placement for ETH DMA descriptors
      ✔ Any working example project (preferably F746G-DISCO)
      ✔ Any documents or references for fixing HardFault in LwIP init

      My Goal:

      Send ADC value as JSON to cloud through Ethernet:

      {
      "adc_value": 1024,
      "device": "stm32f746"
      }


      Any help, guidance, or example code will be greatly appreciated.

      Thank you!




    This topic has been closed for replies.