Has anyone else had issues with DEFINES in LWIP not working right?
So I have run into this a couple of times. Right now I have one that I cannot find a good fix for.
I set SNTP_GET_SERVERS_FROM_DHCP to 1 in CubeMX and generated the project then compiled. It is correctly set in lwipopts.h but in sntp.h and sntp.c it acts as if it is set to zero!
sntp.c has sntp.h and lwip/opt.h included in it.
sntp.h has sntp_opts.h included in it.
sntp_opts.h has lwip/opt.h included in it.
lwip/opt.h has lwipopts.h included in it.
So there's a bunch of nesting of includes and it seems that lwip/opt.h is duplicated in the path to sntp.c.
This seems like an issue with how lwip is set up or a compiler issue... I'm not an expert on this stuff. Anyone have ideas?
Mike.