Having issue in CAN recieve
Hello experts,
I am using stm32f779I - Eval kit, I got stuck in receiving the CAN from other node wheres as transmit from my node is working fine. The IDE and packages am using as follows.
stm cube ide 1.13.1
stm cube mx 6.9.1
package: stm cube F7_v1.17.1
Below is the CAN initialization code I am using
/* CAN initialization */
CAN_FilterTypeDef sFilterConfig;
/*##-1- Configure the CAN peripheral #######################################*/
CanHandle.Instance = CAN1;
CanHandle.Init.TimeTriggeredMode = DISABLE;
CanHandle.Init.AutoBusOff = DISABLE; //
CanHandle.Init.AutoWakeUp = DISABLE; //
CanHandle.Init.AutoRetransmission = ENABLE;
CanHandle.Init.ReceiveFifoLocked = DISABLE; //
CanHandle.Init.TransmitFifoPriority = DISABLE;
CanHandle.Init.Mode = CAN_MODE_NORMAL;
CanHandle.Init.SyncJumpWidth = CAN_SJW_1TQ;
CanHandle.Init.TimeSeg1 = CAN_BS1_6TQ;
CanHandle.Init.TimeSeg2 = CAN_BS2_2TQ;
CanHandle.Init.Prescaler = 6;
if (HAL_CAN_Init(&CanHandle) != HAL_OK)
{
/* Initialization Error */
Error_Handler();
}
/*##-2- Configure the CAN Filter ###########################################*/
sFilterConfig.FilterBank = 0;
sFilterConfig.FilterMode = CAN_FILTERMODE_IDMASK;
sFilterConfig.FilterScale = CAN_FILTERSCALE_32BIT;
sFilterConfig.FilterIdHigh = 0x0000;
sFilterConfig.FilterIdLow = 0x0000;
sFilterConfig.FilterMaskIdHigh = 0x0000;
sFilterConfig.FilterMaskIdLow = 0x0000;
sFilterConfig.FilterFIFOAssignment = CAN_RX_FIFO0;
sFilterConfig.FilterActivation = ENABLE;
sFilterConfig.SlaveStartFilterBank = 14;
if (HAL_CAN_ConfigFilter(&CanHandle, &sFilterConfig) != HAL_OK)
{
/* Filter configuration Error */
Error_Handler();
}
/*##-3- Start the CAN peripheral ###########################################*/
if (HAL_CAN_Start(&CanHandle) != HAL_OK)
{
/* Start Error */
Error_Handler();
}
/*##-4- Activate CAN RX notification #######################################*/
if (HAL_CAN_ActivateNotification(&CanHandle, CAN_IT_RX_FIFO0_MSG_PENDING) != HAL_OK)
{
/* Notification Error */
Error_Handler();
}
/*##-5- Configure Transmission process #####################################*/
TxHeader.StdId = 0x321;
TxHeader.ExtId = 0x01;
TxHeader.RTR = CAN_RTR_DATA;
TxHeader.IDE = CAN_ID_STD;
TxHeader.DLC = 8;
TxHeader.TransmitGlobalTime = DISABLE;
When I tried to debug and check , I understood that am interrupt for once and
when am trying to read the data using below function in interrupt, it is returing with CAN module in reset state.
if(HAL_CAN_GetRxMessage(&hcan1,CAN_RX_FIFO0,&RxHeader,Rx_data) != HAL_OK)
* Interrupt function */
void CAN1_RX0_IRQHandler(void)
{
/* USER CODE BEGIN CAN1_RX0_IRQn 0 */
/* USER CODE END CAN1_RX0_IRQn 0 */
HAL_CAN_IRQHandler(&hcan1);
/* USER CODE BEGIN CAN1_RX0_IRQn 1 */
if(HAL_CAN_GetRxMessage(&hcan1,CAN_RX_FIFO0,&RxHeader,Rx_data) != HAL_OK)
{
Error_Handler();
}
if (HAL_CAN_ActivateNotification(&hcan1, CAN_IT_RX_FIFO0_MSG_PENDING) != HAL_OK)
{
/* Notification Error */
Error_Handler();
}
/* USER CODE END CAN1_RX0_IRQn 1 */
}
Can some one please let me know the mistake am doing.
Thanks & Regards,
R. Srikanth,
Post edited to remove personal information.