Skip to main content
Graduate II
April 20, 2024
Solved

Headers in STM32Cube_FW_U5_V1.5.0 do not contain latest fix in ttps://github.com/STMicroelectronics

  • April 20, 2024
  • 1 reply
  • 1222 views

The headers STM32Cube_FW_U5_V1.5 in still contain the error regarding USB_OTG_GCCFG_FSVMINUS_Msk

    This topic has been closed for replies.
    Best answer by STTwo-32

    Hello @Uwe Bonnes 

    After checking this internally, I confirm that this was solved on the last commit on GitHub (after the release of Version 1.5.0) and it will be updated on other versions (on ST website and Cube repositories) on the coming release. This is already reported on the internal ticket number 170735.

    Best Regards.

    STTwo-32 

    1 reply

    Technical Moderator
    April 21, 2024

    Hello @Uwe Bonnes 

    Thank you for reporting this. Can you give more details about the error. 

    Best regards.

    STTwo-32 

    Graduate II
    April 21, 2024

    Clone https://github.com/STMicroelectronics/cmsis_device_u5.git

    Do "git log -p" :

    -#define USB_OTG_GCCFG_FSVMINUS_Msk 0x1U << USB_OTG_GCCFG_FSVMINUS_Pos) /*!< 0x00000004 */
    +#define USB_OTG_GCCFG_FSVMINUS_Msk (0x1U << USB_OTG_GCCFG_FSVMINUS_Pos) /*!< 0x00000004 */

     

    The last commit fixed the missing opening brace for USB_OTG_GCCFG_FSVMINUS_Msk. No look at STM32Cube/Repository/STM32Cube_FW_U5_V1.5.0/Drivers/CMSIS/Device/ST/STM32U5xx/Include/stm32u599xx.h

    It still has the definition w/o the opening brace

    #define USB_OTG_GCCFG_FSVMINUS_Msk 0x1U << USB_OTG_GCCFG_FSVMINUS_Pos) /*!< 0x00000004 */

    STTwo-32Answer
    Technical Moderator
    April 22, 2024

    Hello @Uwe Bonnes 

    After checking this internally, I confirm that this was solved on the last commit on GitHub (after the release of Version 1.5.0) and it will be updated on other versions (on ST website and Cube repositories) on the coming release. This is already reported on the internal ticket number 170735.

    Best Regards.

    STTwo-32