Hi all! I want to use a STM32G0B1 MCU in both USB device modes: self-powered as well as bus-powered. How does the STM32G0B1 want to detect connection of a host controller to be able to connect/disconnect the DP-pullup?
After reading through DS, RefMan, AN4879 and loads of html/pdf this is what still remains unclear.
-- In the DS this is written: "When VBUS sensing feature is enabled, PA9 should be left at its default state (floating
input), not as alternate function." --> I cannot find this "VBUS sensing feature" anywhere in the Reference Manual.
Is it possible that there is no hardware function for automatic pullup-Enable-after-VBus-sensed? The pin function table does not show this for PA9.
-- Could it be that my STM32G0B1 has to detect a host connection via USB-C lines like CC and so a USB type-B connector cannot be used?
Thanks in advance,
Andreas